Part Number: LMT87 Hi team, I'd like to know about the pin one designator for SOT devices. PCN(20240203000) said current is Pin One Stripe only. The 2 year old device we have is a Pin one Dot. Is this a PCN mistake? BR, Kengo.
Part Number: LMT87-Q1 Dear,
we found there are 2 different shape in the same tape for LMT87QDCKRQ1, and checked many different DC, no matter 21+, 22+ or 23+ all has this issue, so could you indicate if it's general situation?
Part Number: LMT87-Q1 Hi,
What is the expected sensor accuracy, given that it is supplied with a stable supply voltage (5.0 V -+0.1 V), and a temperature range between -40 °C and 100 °C?
to break down the problem:
temp. -50 °C to 40 °C…
Part Number: LMT87 I want to accurately measure the temperature of a surface with the LMT87. To this end, it would be important to place the correct side of the sensor on the surface. The datasheet states: "To ensure good thermal conductivity, the backside…
Part Number: LMT87 Hello everyone,
What was the VDD value used to create the data in Table 3 ("LMT87 Transfer Table") in LMT87.pdf?
I do not see the value of VDD used to create the data in Table 3 ("LMT87 Transfer Table") in https:/…
Part Number: LMT87-Q1 Dear Support,
Good day,
Please confirm why the marking of the middle chip is a little more inclined than the other two chips? Is this normal?
Why does the original product show such a chip marking position? Thanks
Part Number: LMT87 Other Parts Discussed in Thread: LMT84 , Hello,
I recently changed a design from the LMT84DCKT to the LMT87DCKT
However, with the LMT87DCKT I am getting an output of 887mv at 27 Celcius?
It should be 2271mv? at 27 Celcius?
The LMT87DCKT is…
Part Number: LMT87-Q1 Other Parts Discussed in Thread: LMT87 , Please tell me. I'm using LMT87 now. However, the pcb will corrode in under adverse conditions and the LMT87 will not work. In this case, is it okay to have a moisture-proof coating on the…
Part Number: LMT87-Q1 Dear team,
Could you help to check leakage current for below?
Part. No
Temp. (DC 14V)
Leakage Current
LMT87QDCKRQ1
+ 125 ︒ C
+ 25 ︒ C
- 40 ︒ C
Thank you.
BR, Hannah.
Part Number: LMT87-Q1 Hi,
In LMT87-Q1 datasheet, Figure 10 shows the capacitive load(Cload) should be less than or equal to 1100pF. But If the capacitive load greater than 1100pF(for example: 0.022uF) without a series resistor , What will be the impact…