Part Number: LMV431 Hi TI Team,
Thank you for your support.
I have a question for part LMV431CM5X/NOPB .
*Is this part contained material used Panasonic material (Yes. as Material Vendor also)?
I don't think so. But it is just make sure Y/N type question…
Part Number: LMV431 Hi Team,
What's the operating virtual-junction temperature Tj range? -40~150C? Only operating temperature can be found in datasheet. Or I need use thermal resistance to calculate. Thanks.
BRs,
Francis
Part Number: TLVH431 Other Parts Discussed in Thread: LMV431 , , LM431 I am doing a bench test comparison of the TLVH431CLPR versus LMV431 voltage shunt devices.
The component test using the circuit below resulted in Vref = 1.24v and Vout = 2.5v as expected…
Part Number: LMV431 Other Parts Discussed in Thread: TINA-TI , TL431LI Hello,
I've played around with this and haven't come up with a good solution yet. I have a project that is battery powered (nominal 12V - 24V) but when the battery is removed I want…
Part Number: UCC28C42-Q1 Other Parts Discussed in Thread: LMV431 , TL431 , UCC28C42 Hi Team,
We would like to ask your help regarding the customer's inquiry below.
When I design the UCC28C42QDRQ1 with Webench the adjustable precision shunt regulator…
Part Number: LM5117 Other Parts Discussed in Thread: LMV431 Hello,
This is related to a previous question where it was suggested to use a zener in series with the LMV431 to increase the clamp voltage beyond the specifications of the LMV431 to 42V to allow…
Hi Neo,
thanks for the update.
So it looks like some disturbance is getting injected on to the FB/REF input of the LMV431 but this should not be a loop stability issue.
This issue could be due to:
- LMV431 being placed very close or below the inductor…
Part Number: LMV431 Other Parts Discussed in Thread: TLVH431 Hi team,
The available model for LMV431 seems to concentrate only on DC behavior. Is there an available Spice simulation model that models the correct .TRAN and .AC behavior?
Thanks,
Obinna. …