Part Number: LMX2492-Q1
Hi,
When reading table 7.6 of the LMX2492-Q1 datasheet, the following question arises:
What is the frequency range that I can use on pin fOSCin if the signal is single ended ?
I think that there is no problem in using the following…
Part Number: LMX2492-Q1 Other Parts Discussed in Thread: LMX2492 Dear expert,
Can Vcp and Vcc of LMX2492 share same LDO with other device like MCU?
Thanks
Part Number: LMX2492-Q1 Other Parts Discussed in Thread: LMX2492 Dear expert,
Is there specific power ripple requirement for power supply for LMX2492?
thanks
Part Number: LMX2492-Q1 Hello,
I am working in a frequency synthesizer, and I'm trying to model its behaviour with ADS keysight. However, my results are not very accurate compared to real behaviour of the PLL.
Could you provide any aid in modeling…
Part Number: LMX2492-Q1 Other Parts Discussed in Thread: LMX2492 Team,
We are trying to figure out if we can delay the output clock by up to 10ns. Can you advise?
Thank you.
Part Number: LMX2492-Q1 Hi All,
Do you have any information impedance of the Fin and Fin* vs frequency?
I can't find any data impedance of the Fin and Fin* vs frequency in data sheet, but impedance matching is mentioned at layout guide.
Thanks and…
Part Number: LMX2492-Q1 Other Parts Discussed in Thread: LMX2492 , LMX2491 Dear All,
I would like to generate ramp frequency waveform as bellow;
- Ramp repetition frequency: 100 kHz
- Start frequency: 1 GHz
- Stop frequency: 3 GHz
- Frequency repeatability…
Part Number: LMX2492-Q1 Other Parts Discussed in Thread: LMX2492 , CODELOADER I'm attempting to use the hardware ramp function of the LMX2492-Q1. I am able to lock the device to a 100 MHz reference signal and produce a clean output. I can easily change…