Part Number: LMX2571 Other Parts Discussed in Thread: LMX2572 Hi,
According to the datasheet, "The switch can also be configured as a 1:2 fanout buffer, providing the signal on both outputs at the same time."
What is the time difference between…
Part Number: LMX2571 Hi,
It's not entirely clear from the datasheet. Can RFoutRX and RFoutTX be configured to output different frequencies simultaneously? Section 7.3.10 states that the "active port" can be switched as well as the frequency. What does…
Hello Vicente,
Thanks again for the help in solving a complex issue. To close the loop, I've marked your first response as the correct one as the issue was on the OSCIN pin.
For anyone else reading, it was not straight forward though: My CMOS oscillator…
Part Number: LMX2571 Hi Team,
I would like to know FSK input pin condition while POWERDOWN.
I'm planning to share I2S signal with LMX2571 and other devices.
When LMX2571 is in POWERDOWN mode, is the voltage of I2S signal droped by LMX2571?
In addition…
Part Number: LMX2571 Other Parts Discussed in Thread: CODELOADER , LMX2571 is used in synthesizer mode with internal VCO in our application.
Using Codeloader to config the LMX2571, the Auto Reload with Changes has been ticked.
- If PLL_R_PRE_F1 = 1, registers…
Part Number: LMX2571 Hi Team,
My customer plans to use LMX2571 and their DSP chip in their walkie-talkies. The DSP supports SPI and I2S mode. Can you help explain the differences between these two FSK mode? And any considerations for their applications…
Part Number: LMX2571 Hi,
I would like to generate an FSK signal with a 1 Mbps data rate; hence, I need to increase the loop bandwidth to a few MHz. However, the internal capacitors of the integrated loop filter impose a limitation on the loop bandwidth…
Part Number: LMX2571 Hi team, Looking at the modulation scheme of the LMK2571, it is 3-bit FSK. Is it possible to transmit voice on the carrier wave like a transceiver? BR. Kengo.
Part Number: LMX2571 Hi Team,
From the datasheet, LMX2571 can be used with an external VCO. To that end, a dedicated 5V charge pump and an output divider are available for this configuration.
But I want to use a VCXO operating at 3.3V as an external VCO…