Part Number: LMX2581EVM Other Parts Discussed in Thread: LMX2581 Request review materials for product design.
LMX2581 Evb Design Source.
Ideally gerber files and, if possible, a step 3D of the board.
Thanks
Part Number: LMX2581EVM Other Parts Discussed in Thread: USB2ANY , Hi,
I have a new LMX2581EVM and USB2ANY programmer im using to generate a 3.5 GHz Signal (RFOUTA) and a 125 MHz Signal (RFOUTB). The output of either channel seem fixed at 3.89 GHz regardless…
Other Parts Discussed in Thread: CODELOADER , USB2ANY No RF Output with default configuration.
Board draws nearly 84mA current when connected to 3.3V DC.
TICS pro and CodeLoader are both used and are establishing connection with USB interface device connected…
Part Number: LMX2581EVM Other Parts Discussed in Thread: CODELOADER , , LMX2581 Hello TI experts,
My customer now tests LMX2581EVM with CODELOADER software, and there is one problem.
output frequency range is 50 to 3760MHz is datasheet. but if I change…
Part Number: LMX2581EVM Other Parts Discussed in Thread: LMX2581 , CODELOADER , USB2ANY Hello,
I am having trouble getting any RF signal out of the LMX2581EVM.
The hardware has been reconfigured to take a reference signal from an external clock at 10 MHz…
Hi Noel,
Thanks for the advice. The 100MHz (XO) on the LMX2581EVM has been stopped. I mounted a resistor so that 10MHz/0dBm (from SG) can be supplied from OSCin on the board to LMX2581 (pin 29). (R13: 0Ω, R14: not mounted, R15: 51Ω, R16: 0Ω)…
Part Number: LMX2581EVM Other Parts Discussed in Thread: LMX2581 , , LMX2572LP , LMX2572 Hi, I would like to build frequency tunable oscilator in range 2-3 GHz with one temperature stabile output. I want to use LMX2581. Is these chip sutable for this aplication…