Part Number: LMX2582 Other Parts Discussed in Thread: LMX2820 , LMX2594 Hi,
I am looking at using the LMX2582, I am curious if anyone has pushed the LMX2582in terms of freq. change speed (i.e. times it takes to write frequency change to proper registers…
Hi Noel
I had like to confirm whether it's preferable for an OCXO to have a CMOS output or a Sinewave output as a reference clock to LMX2582.Since we are planning to get a precise output like less than 100Hz variation of signal from LMX output.
Part Number: TRF3765 Other Parts Discussed in Thread: LMX2582 Hi Team,
We are in the process of selecting a PLL with VCO that can generate an output frequency programmable from 900 MHz to 2.45 GHz to achieve low phase noise and jitter, we are evaluating…
Part Number: LMX2582 Hello, To support a full assist at LMX2582, I do not find the following register or bit name described app note snaa336a.pdf. VCO_CAPCTRL_FORCE VCO_DACISET_FORCE VCO_DACISET Are those register or bit names as follows at LMX2582…
Hi team,
I am programming using NODE MCU (ESP8266)
We Verified the functionality of LMX2582 using Tics pro software .Its working fine .
But we are unable to lock the frequency using Node MCU (only default frequency we observed)
It would be helpful if…
Part Number: LMX2582 Other Parts Discussed in Thread: LMX2594 , LMX2820 Hi,
we employ frequency scan in our application. Every time the synthesizer calibrates frequency, it's phase randomly shifts (180, 120, 90 degrees depending on frequency). There is…
Part Number: LMX2582 Hi Team,
I have a question for LMX2582, is phase programmable in integer mode? Like 40MHz input, and the output is the same frequency, but phase is shifted? And what’s the relationship between input and output? Thanks a lot!…
Part Number: LMX2594 Other Parts Discussed in Thread: LMX2582 , LM2594 I am planning to drive an LMX2594 with an LMX2582 (around 260MHz) . What would be the preferred connection between LMX2582 output and LMX2594 input. Most optimum to me seems not using…
Part Number: LMX2582 SIR
I Want to use LMX 2582 FOR MY PHASE FREQUECNY DETECTOR APPLICATION.
MY REF INPUT FREQUENCY IS 56 MHz.
AT THE RFOUTPUT A AND RFOUTPUT B, I NEED DC VOLTAGE OUTPUT FROM 0 V TO 8 V.
CAN I ACHIEVE THIS.
PLEASE GIVE US THE GUIDANCE…