Part Number: LMX2592 Other Parts Discussed in Thread: LMX2594 Hi team,
i'm using the LMX2592 for the new project.
I have to jump between 2 frequencies from 4.95 GHz to 7.15 GHz with the minimum lock time.
I attach the register map for the 2 frequencies…
Part Number: LMX2592EVM Other Parts Discussed in Thread: LMX2592
According to the datasheet of LMX2592 Fig 6-12, the output power is nearly constant for all the frequencies.
But when we try to sweep across frequency with these settings, we are not able…
Part Number: LMX2592 Other Parts Discussed in Thread: LMX2594 , LMX2595 Hi,
My customer have interesting about the LMX2592, LMX2594, LMX2595.
Which one do you recommand use in new project.
Thanks!
Jeff
Part Number: LMX2592 Hi
I do have a question regarding the different Datasheet Revisions for the LMX2592 (latest greatest is Rev. G).
Does the Datasheet Revision correspond to a HW Revision of the Chip? I.e. are there different HW Revisions of the Chip…
Part Number: LMX2592 Other Parts Discussed in Thread: LMK05318B Hello,
My customer is looking for a PLL device with the conditions below.
- Ref Clock : TCXO 10MHz or GPS (1PPM)
- Output clock : 6.3~6.9GHz
They prefer products that allow them to select…
Part Number: LMX2592 Other Parts Discussed in Thread: LMX2594 , Hello team,
My customer has some experience with LMX2594, and now considering to use LMX2592.
Is it possible to use same register setting as LMX2594? I have checked up to register 7, but I see…
Part Number: LMX2592 We've been using the LMX2592 Synthesizer for several years. Looking at the RF power output in detail, we see shifts in the output at ~1200MHz to 1700MHZ & 3400MHZ. We assume this is due to different internal VCOs being used. I have…
Part Number: LMX2592 Dear Sir,
I am using LMX2592 for 4.3GHz freq generation, I tried fractional method lot of spurs which is multiple of 50MHz and and multiple of around 22MHz are seen. Later I tried Integer method , spur levels got reduced. But still…