Part Number: LMX2594 I am using the LMX2594EVM right now and I am trying to replicate frequency hopping, however I have noticed that when I change frequencies (N, NUM, DEN) I need to disable the output otherwise I get weird products while the registers…
Part Number: LMX2594 Hi Noel,
My customer want to generate a spread Spectrum clock.
Input 100MHz
output Frequency: 194~206MHz
ramp time:10ns level.
similar to figure10 in datasheet,is that possible to realize a ns level ramp time?
thanks.
BR,
Victor
Part Number: LMX2594 Hi all,
I have a question about the SYNC Category:if chdiv<512 and M=1 and Fout is multiple of the input frequency,does it mean the output of two lmx2594 phase aligned?
Part Number: LMX2594 Hi
We are trying to implement the "FULL ASSIST" mode for the LMX2594.
This is the registers list we program, but we didn't get any results:
x"240488" - reg 36 chose the frequency
x"002414" - reg 0…
Part Number: LMX2594 Other Parts Discussed in Thread: LMX2820 Hello,
Could you please suggest the possible ways to improve the Turn ON time of the LMX2594 PLL chip with below requirements.
Normally the locking time of the PLL chip was combination of VCO…
Part Number: LMX2594 Other Parts Discussed in Thread: LMX2820 Hi team
1. Is it OK to use the clipped waveform as the input signal of this device. For instance, I assuem the TCXO as below. Could you tell how the device performance e.g. jitter, spurious…
Part Number: LMX2594 I'm using the #1Nos LMK04828B and #2Nos LMX2594RHAR in my design to provide #4Nos phase aligned sampling clocks from LMX to my device.
I referred some EVK and mapped the LMK to LMX as shown in the attachment. And i have some…
Part Number: LMX2594
Hi Team,
There is a section I didn't understand in the datasheet 7.3.13.2 describing the maximum slew rate of the automatic ramping must be kept less than 250kHz/us.
The example given 7.3.13.2.2 just below this section shows…