Part Number: LMZ31506 used two LMZ31506,frist LMZ31506 PWRGD pin could drive the second LMZ31506 INH/UVLO?
INH/UVLO pin could direct connect PWRGD pin?
Part Number: LMZ31506 The board was working fine, but at some point the LMZ31506RUQR's VOUT output (+3.3V) went to 0V.
・When I measured the resistance value between VOUT and GND after it became 0V, it was 1.9Ω. ・The resistance value between VOUT…
Part Number: LMZ31506 Other Parts Discussed in Thread: TPS84621 , TPS84620 , TPS82130 LMZ31506のスロースタートについて教えてください。
LMZ31506のデータシートの9.16 Slow Start (SS/TR)にて、時間とコンデンサの定数の関係についてTable6に記載されていますが、計算方法はどこに記載されていますか?
データシートは下記リンクを参照しております。 www.ti.com/.../lmz31506…
Part Number: LMZ31506 When LMZ31506 startup, power good output is delayed about 6ms.
Please refer below waveform;
※ch1: Vin (5V), ch2: Vout (1.03V), ch3: PWRGD
Is there any reason for PWRGD delay?
If there detailed schematic, please let me e-mail address…
Part Number: LMZ31506 We're using an LMZ31506RUQ to generate 1.0V from 5.0V - which it is doing - and then using the PWRGD output of that device to enable 2 LMZ31503RUQ's,1 LMZ31503RUQ, and 1 TPS7A8801RTJ. However, the outputs of these sequenced devices…
Hi Ibram,
What matters more than what is the amplitude of the noise is the frequency content of it.
Here is an application note that discusses synchronization between different DC/DCs is order to prevent beat frequencies.
https://www.ti.com/lit/pdf/s…
Part Number: LMZ31506 Other Parts Discussed in Thread: LMZ31503 , TPS54320 Greetings, we are attempting to track a 1.8V turn on (LMZ31506) to a 3.3V turn on (LMZ31503). The resistors we've calculated are R1 = 37.8K and R2 = 18.9K. Unfortunately this results…
Part Number: LMZ31506 Could you tell us about the PWRGD terminal specifications of the LMZ31506RUQR?
There is a description of the TYP value for the PWRGD threshold, but there is no description of the Max value and Min value.
Could you tell me about the…
Part Number: LMZ31506 Other Parts Discussed in Thread: LMZ31710 , Can INH / UVLO pins be used with 0V / + 3.3V active controls (CPLDs, power sequencers, etc.) instead of open drains?
In this case, a pull-down resistor (about 1k to 10kΩ) is connected to…