Part Number: LMZ31707 Hello.
I have a problem about operation of LMZ31707.
This circuit used to operate normally.
but there has been an malfuction.
Green is SS/TR Voltage. not working.
Insert the capacitor on the outside to perform normal…
Part Number: LMZ31707 Hi Expert,
I am using LMZ31707RVQ. PWRGD seems sensitive if a sudden load turn-on on its output after it's startup. Can I use a RC network to sense+ pin to decrease the sensitivity like other DC/DC converter? such as 100ohm series…
Part Number: LMZ31707 Hello there,
Two questions:
1 - For testing purposes on my application, I will have the LMZ31707 supplying 1.7, 1.8 and 1.9 V. I am looking at Table 2, 'Standard R_set Resistor Values', on page 11 on the datasheet and the R_rt…
Part Number: LMZ31707 Other Parts Discussed in Thread: LMZ31710 Dear team,
Our customer will changes the circuit which they designed in LMZ31710 to LMZ31707. Is there the problem?
Regards, PAN-M
Part Number: LMZ31707 From datasheet table 8, I want to set UVLO at 10V turn-on, and 9.5V turn-off so I select 68.1K/9.31K resistors for Figure 40.
Since my PVIN is from a battery source, I want to limit the leakage current to increase to 681K / 93…
Part Number: LMZ31707 What is the ELV number of the LMZ31707RVQT? I contacted the Customaer Support Center with CS0552385, but they answered to contact E2E.
Part Number: LMZ31707 Hi,
I'm looking to implement a status LED on the PWRGD pin of a LMZ31707RVQ. Are there any default configurations from TI for this? If not, can you provide some recommendations? The datasheet notes a pullup resistor (10k-100k)…
Part Number: LMZ31707 Hi all,
A customer recently approached me regarding the UVLO level for this device.
The datasheet says that the UVLO level is 4.5V internal. Does that mean with no external resistors and the UVLO pin left floating, the device…