Part Number: LMZ31710 We have a configuration where the STSEL pin was unintentionally left open.
An additional capacitor has been connected from the SS/TR pin to ground.
In this configuration, will the device operate with the current source charging the…
Part Number: LMZ31710 The reference design for the LMZ31710 has the power arranged over a 4-layer PCB. How critical are the dimensions between the 4 layers for the function of the regulator? If critical, what are the stackup requirements for this regulator…
Part Number: LMZ31710 When checked the connection between AGND and PGND with a tester, it found that 2-pin AGND was open and 23-pin AGND was shorted.
In other E2E threads AGND and PGND are supposed to be connected internally, but would you let me know…
Part Number: LMZ31710 Other Parts Discussed in Thread: TPS84A20 , The other E2E thread are described that LMZ31710 and TPS84A20 are compatible, but absolute Maximum Ratings of Vout is differ.
・LMZ31710: 10V_max
・TPS84A20: 6V_max
Please let me know the…
Part Number: LMZ31710 Other Parts Discussed in Thread: LMZ31707 , LMZ31704 Hi team,
The thermal resistance of LMZ31710 does not match the notes. LMZ31704 and LMZ31707 in the same series are defined by Θja, Ψjt, and Ψjb. What is the correct…
Part Number: LMZ31710 Hi Team,
On customer PCB, LM31710 is very close to a screw hole. The diameter of screw hole is 3.5mm. The distance from the edge of module to the center of screw hole is 5.5mm. Customer concerned about the stress issue. So I was…
Part Number: LMZ31710 Hi -
Anyone else ever have a problem where the switch node (PH) stops switching and the regulator won't fully come up to voltage?
I'm making VOUT = 1.0V from VIN = 5.0V and after about 2.5ms, VOUT is only about half-way up…