Part Number: LMZ35003 Hi team.
When VOUT=12V, is it possible to set Slow Start to a short time such as 7ms?
The data sheet says 17ms (SS/TR=22nF) is recommended, but why?
Part Number: LMZ35003 Hi All,
I have a question about the output ripple of the LMZ35003.
Please tell me the values of the input and output capacitors in the graph below.
Best Regards, Ishiwata
Part Number: LMZ35003 Hi All,
I have a question about slow start. It is stated that the SS pin must be open at 5V or less, but is it possible to set the SS time to 17msec by connecting a 22nF capacitor when the output voltage is 5V?
Best Regards, Ishiw…
Hello Hans,
Getting back to you a little late, but we require the receipt of purchase from authorized distributor, as well a picture of the reel to support this claim.
Part Number: LMZ35003
Hi team,
What is the minimum capacity of the output capacitor of LMZ35003?
There is a description that it is 47uFx2 of Ceramic capacitor, but if it is 10.5Vout,
the capacity reduction of DC bias is large and I do not know how many…
Part Number: LMZ35003 Hello,
We are unable to procure the LMZ35003RKGR and were wondering if the TPS84250RKGR was an acceptable alternative or if there were better alternatives TI offered.
THanks!
Adam
Part Number: LMZ35003
Hi,
I am using the LMZ35003 in a design that operates off 15-50v from lipo batteries to control 12v LED lights. I have built around 25 units to test with and out of those I have seen 4 failures where the LMZ35003 is blown. In these…
Part Number: LMZ36002 Other Parts Discussed in Thread: LMZ35003 , Hello team, I have a question about LMZ36002 and LMZ35003 Light Load Operation. Do LMZ36002 and LMZ35003 operate in pulse skip mode at light load when we use the external clock synchronization…
Part Number: LMZ35003 Other Parts Discussed in Thread: LMZ13608 To Whom It May Concern,
Please let me know about the latest temperature profile of LMZ35003.
According to the datasheet link, the following file is the temperature profile.
[Data Sheet…