Part Number: LMZM23601 Hi Ti,
We are considering LMZM23601 with the following configuration: Module Type=Adjustable Vin=24V Vout=5V Mode=FPWM
With this configuration, the output may become unloaded. Is this a problem?
Is a bleeder resistor or similar…
Part Number: LMZM23601 Tool/software: Hello,
I am using LMZM23601 in inverting buck-boost configuration:
Vin: 12V
Vout: -5V @ 0.5A.
I designed the circuit from Webench simulation, now I have the real design as prototype but the -5V output is not…
Part Number: LMZM23601 Other Parts Discussed in Thread: TPSM365R6 ,
Tool/software:
LMZM23601 is not recommended for new designs but it seems like the replacement part (TPSM365R6) needs two more resistors and a capacitor as minimum requirements. Is…
Part Number: LMZM23601 Other Parts Discussed in Thread: PSPICE-FOR-TI Hi, Dear product line
my customer configure LMZM23601 as a inverting regulator as below figure shows.
then customer find he could not disable LMZM23601 with a FPGA_IO directly…
Part Number: LMZM23601 Tool/software: hi
i am looking fo a poin competible IC for LMZM23601SILR
with highe current rating
the high input voltage doesnt really matter for me i am looking fo arround 15V input to 11 V output
Part Number: LMZM23601 Hello, would you know the line regulation and load regulation (voltages) for this component? Could you please state the values and guide me to where it is in the specification. I saw something close on page 28, but it is for the…
Part Number: LMZM23601 Other Parts Discussed in Thread: LMR60410 , TPSM33615 , , Tool/software: Hi support team,
When the output voltage is 8V and the input voltage is 9.5V, the PFM operation switches to PWM operation. This causes the input current…
Part Number: LMZM23601 Other Parts Discussed in Thread: TPSM33625 Tool/software: Dear Sirs and Madams,
We are currently verifying the operation of LMZM23601.
VOUT:8V
IOUT:2.5uA
Currently, for all products, when VIN is 9.6V, the input current…
Part Number: LMZM23601 Tool/software: I accidentally break one of the capacitor soldered on the top side of the component. Is there any information of the capacitor value so I can repair it?
And if it is possible I would like to know the relative schematic…
Part Number: LMZM23601 Tool/software: Hi support team, I would like to calculate the TJ of LMZM2360x using ΨJT.
Is the temperature measurement point in the center of the top surface of the package around the PICK AREA in the diagram below?
Regards…