Part Number: LP2951-N Other Parts Discussed in Thread: LP2951 Hello,
This is a question relating to Thermal Shutdown of an LP2951-N LDO regulator.
We are trying to debug an issue we have with site failures of a number of our devices. Another manufacturer…
Part Number: LP2951-N Other Parts Discussed in Thread: LP2951 Hi all,
LP2951CMM-3.0/NOPB with this part can I get adjustable output of 15V instead of fixed output 3V. If yes please guide me in pin connections and what happens with internal resistor…
Part Number: LP2951-N Section 8.1 of the datasheet indicates that when SHUTDOWN is pulled low, the regulator is turned off. This disagrees with the rest of the datasheet. Is this a typo?
Part Number: LP2951-N Other Parts Discussed in Thread: LP2951 Dear Team,
according to datasheet it is allowed to leave SHUTDOWN IN pin floating.
Is it the same for LP2951 (not the N version)?
Regards
Andreas
Part Number: LP2951-N Other Parts Discussed in Thread: LP2951 When pulling the LP2951 shutdown pin low to disable the regulator, we noticed that the error (open collector output) pin is being pulled low. Does the error detection comparator circuit stay…
Hi Ian,
LP2951-N was originally released by National Semiconductor before TI acquired the company. The LP2951 is the version of the device that was released by TI while the two companies were competitors.
Very Respectfully,
Ryan
Part Number: LP2951-N Team,
my customer is using LP2951ACMM-3.3. Nominal Vin is 10V.
As part of failure considerations, they would like to know the behavior of the device when abs max Vin is exceeded -> Vin =38V It's ok for the device to be destroyed…
Part Number: LP2951-N Hi
LP2951ACSDX/NOPB is this the right part for the 5V fixed output voltage in WSON Package? if not please suggest, I am looking for LP2951-N in WSON 5V fixed output voltage.
Best Regards
Umesh Thapa