Part Number: LP2985 Tool/software: Kindly provide below listed parts life cycle status. How long expect to continue manufacturing it?
Sr No
Description
Make
MPN
1
IC LM78L12ACM fixed voltage regulator 100mA SO8
Texas Instrument…
Part Number: LP2985
Tool/software:
Hello, I'm using the LP2985-50DBVR in one of my designs to achieve a 5V fixed output, however when there's no load connected before applying an i/p voltage , I am seeing 10V. When I attach the load before applying…
Part Number: LP2985 Tool/software: Hello,
In the datasheet of LP2985-33DBVR, In fig 6-34, the ground pin current is shown. Just wanted to understand what is the impact of high ground pin current?
Thanks
Madhurani
Part Number: LP2985 Dear team Regarding the product: LP2985IM5X-4.0/NOPB, we found that the ones produced in 2025 have no markings on the bottom. Are they discontinued? Is there any difference in their performance? We observed that the products without…
Part Number: LP2985 Tool/software: Hi,
We use the LP2985-33DBVR in our mass prodcut, and now, we use two batchs goods in our production line( Datecode 2222+5 and 2421+5),
Now, the 2222+5 datecode is normal for the voltage drop, and the 2421 +5 datecode…
Part Number: LP2985 Tool/software: Dear team,
Is there any plan to make LP2985-10DBVR M3 version?
If not, Is there EOL plan of LP2985-10 device? Please let me know your opinion.
Thank you.
Part Number: LP2985-N We noticed a failure in precision of our analog output circuit. The circuit includes a voltage-Regulator type LP2985AIM5-3.3/NOPB.
Comparing Initial-measurements (2023) and up-to-date measurements, we found out, that the output…
Part Number: LP2985 Tool/software: Hello,
I have a question regarding part numbers LP2985IM5X-3.3/NOPB and LP2985IM5-3.3/NOPB. I'm not sure, if they stand for legacy chip (tolerance of 1.5%) or new chip (tolerance of 0.5%).
Thank you in advance!
Part Number: LP2985 Tool/software: Hi support team all.
I have received an inquiry from my customer.
The inquiry relates to PCNs issued in December 2022 and September 2023.
・Is LP2985-50DBVR (Richardson production in 2024) a legacy spec in the…