Part Number: TLV767 Other Parts Discussed in Thread: LP2989 ,
Hi LDO Folk,
For 12VIN 5VOUT 300mA condition, what would be the best option - TLV767 vs LP2989?
It looks no significant noise performance difference between them as below. TLV767 is the newer…
Part Number: LP2989 Hi team,
my customer would like to know the dropout characteristics of the LP2989-5V variant. Ideally, he would like to see the plot below for the 5V version.
If this is not possible, can someone comment on whether supplying the LP2989…
Part Number: LP2989 Other Parts Discussed in Thread: TPS767 , TPS777 Hi team,
my customer is using the LP2989IMX-3.3 in 8 SOIC package at 3.3V with enable feature.
do we have any drop in p2p devices that can source 0.8-1A?
Thanks,
Kevin
Part Number: LP2989 Is there a limit on max output capacitor for LP2989 ? Customer has max load capacitor of 180uF which include ceramic and electrolytic, is that acceptable ?
Or will it be only decided by Stable Region for Output Capacitor ESR (figure…
Part Number: LP2987 Other Parts Discussed in Thread: LP2989LP2989AILD-3.3/NOPB is EOL. I'm looking to use LP2987ILD-3.3/NOPB to replace LP2989AILD-3.3/NOPB. Output current 200 mA is enough in my design.
As the pin 2 has no connection on my current…
Part Number: LP2989 Hi, we've been reviewing the datasheet for the LP2989 (we're using the LP2989IMM-5.0/NOPB), and in some places, it's saying the minimum input voltage is 1 volt higher than the output voltage, but in other places (e.g. Section 6.5)…
Part Number: LP2989 Hi,
can you please help with your assessment: for LP2989AI-3.3, Vin 5V, Iout 0.05-0.1A, Temp -40 to 85 degC use-case, is output tolerance really up to -4% according to the datasheet, so possibly going down to 3.168V?
Regards,
Andr…
Part Number: LP2989 Hello,
I'm trying to use LP2989 with 8SOIC packaging, but the layout footprint is missing on the datasheet. It's risky to come up with my own version of layout. Is there any where I can get that information?
Thanks,
Jie
Part Number: LP2989 Hello,
I have a LP2989AILD-3.3 on a board (WSON package), and the component output fall to 1V when the ambient temperature up to 70°C.
The output can stay to 1V for hours with a temperature of 25°C and return to 3.3V.
The…
Part Number: LP2989
Dear Sir,
I am using LP2989 for our power board but I can' find S/D (SHUTDOWN) pint Max voltage rating value in the datasheet.
A little bit urgent for this case, may help provide to me ? Thanks.