Part Number: LP3855-ADJ Hi Experts,
Good day.
I want to clarify the recommended output voltage of this LDO device, LP3855-ADJ.
TI website shows 6.6Vout max but I couldn't find it from its datasheet . We are actually looking for an LDO device that…
Part Number: LP3855 Hi Support team,
I need to ask this question because the data sheet is specifying that there be a 10k pull up on the enable pin. This values is specified multiple places in the data sheet. Why do i need a pull up and can i connect…
Part Number: LP3855-ADJ Hi, Good day. I hope everything is fine. Our customer is looking for the thermal information/resistance of LP3855EMP-ADJ/NOPB (SOT-223-5 Package) as we cannot find this information on the datasheet. I would appreciate if you could…
Other Parts Discussed in Thread: LP3855-ADJ I'm using the LP3855-Adj with a 6 Volt input, and trying for an output voltage of 5.6V. The output never goes above 5.4V, though I can adjust it lower. I've try both increasing and decreasing the input voltage…
Other Parts Discussed in Thread: LP3855 , LMP8646 Hi -
I'm currently using an LP3855 for a 5V output with loads varying from 2A-100mA. I want to limit the load to 1A partly to prevent the regulator entering the overcurrent protection, partly to protect…
Part Number: LP3852 Other Parts Discussed in Thread: LP3855 , TPS7A45 , TPS740 Dear Team,
I am using LP3852 in one of my application.
I/P 7V output 5V, Maximum current drawn from output is 1A. Below is my schematic.
May I know your comments/Suggestions…
Hi Jones
After bring in my first question into this forum, I always appreciate your kindness.
I could not understand that the cause of output voltage drop on LP3965-ADJ seems to be the level of /SD pin,
And I replace it with LP3855-ADJ in the…