Part Number: LP38690 Hello E2E Experts,
Good day.
HBM is given on the datasheet, however, I would like to ask: What is the CDM ESD sensitivity of the LP36890 voltage regulator?
Thank you in advance.
Regards,
CSC
Part Number: LP38690 Questions about footprints.
Please tell me the positional relationship between the parts and the land pattern.
The positional relationship is unknown in the data sheet.
TO-252 Package
NS Package Number TD03B
Part Number: LP38690-ADJ Other Parts Discussed in Thread: LP38500-ADJ , , TPS7A8101-Q1 , TLV767-Q1 , TPS74801-Q1 , TPS7A54-Q1 , TPS7A52-Q1 Hi,
I'm looking for a regulator with the same pinout as the DFN6 package of this device, but with VO at least able to…
Part Number: LP38690 Hello,
My customer is using LP38690SD-3.3/NOPB for the optical module application.
The following defect occurred in LP38690SD-3.3/NOPB while using the optical module.
- Input voltage = 5V, Typical load current = 230mA
- The output…
Part Number: LP38690-ADJ Hi , I'm using this part LP38690SDX-ADJ, with a 6.3V in and 5V out. My top feedback resistor is 30.9k, and bottom feedback resistor is 10k. I'm using a 4.7uF input and output ceramic cap.
Upon measuring the output,…
Part Number: LP38690 Hi,
I would like you to confirm whether spec of load regulation is correct or not.
Because, max of load regulation is 5V in worst case.
I think this is too big, so could you confirm about above ?
BR,
Part Number: LP38690 Hi,
The LP38690 shows the SNS input stage to use an internal resistor divider R1/R2, but it does not spec the resistor values or input leakage. How large is the internal resistance R1+R2, and is there any other leakage spec? I am…
Part Number: LP38690 I have a customer who is using a LP38690 with Vin = 6.6V from a 400kHz switching power supply and Vout = 5.0V. They are using a 4.7uF ceramic capacitor on the input and both a 4.7uF, 0603 located right at the output pin of the part and…
Other Parts Discussed in Thread: LP38690 HI
Does LP38690 have any specification for slew rate of the input voltage?
Our customer are going to put the resistor for current limiting resistor on the input line. ( under dozens ohm)
It will be concerned with…