Part Number: LP38693 Hi,
I am using LP38693QSD-5.0/NOPB. I would like to know what is the maximum allowable capacitance at the output since I am connecting this 5V to multiple loads. each one has some decoupling capacitance. So I would like to know what…
Part Number: LP38693 Other Parts Discussed in Thread: TPS7B7701-Q1 Hi TI support,
I am looking for an voltage regulator whith an output voltage of 5V and the load current is 100mA. The required output voltage tolerance is 2% under all conditions like over…
Part Number: LP38693-Q1 I am conducting the FMEDA for an ECU that uses LP38693QSD-3.3. Please may I have the component fit rate as per SN 29500 and the FMD aswell.
Thank you,
Bushra
Hi Mohamed,
This part has been shipping parts continuously going back 5 years so I don't know what you mean about wanting a "reactivation reason". We have issued a Life Time Buy period for this device, after which the device will be obsolete.…
Part Number: LP38693
[Case:612982]Technical Data Inquiry for our customer.
SiliconExpert is contracted by our customer to work with their suppliers for accuracy and compliance purposes.
Could you please provide us with the reactivation reason as the part…
Part Number: LP38693 Hi Support Team.
Reliability data of LP38693MP-5.0/NOPB cannot be confirmed.
Please tell me the result of the latch-up test for LP38693MP-5.0/NOPB.
Thanks,
Part Number: LP38693-ADJ The design from "Using LDO for LED Control and Brightness Matching" adds resistor divider R1 and R2 to increase the voltage across R3 to 2V. What is the advantage of this, compared to simply connecting ADJ to R3 and…
Part Number: LP38693-ADJ Other Parts Discussed in Thread: LP38693 , TPS7A49 The datasheet claims that LP38693-ADJ has noise of 0.7uV/(Hz-2). Is that number correct ?
I need low noise for analogue circuitry and I was considering LP3878MR-ADJ first.
LP38693…
Part Number: LP38693-ADJ Hi,
I am starting a new project which will need LP38693-ADJ.
I have read the datasheet but I don't see description on how will this LDO behave under over current or short circuit condition.
If the Output pin is shorted to…
Part Number: LP38693 Hi,
We are using LDO (Part number - LP38693MP-5.0/NOPB) in our project but maximum input voltage of this LDO is 10V. We need >12V max input voltage so please recommend the part ASAP.