Part Number: LP3878-ADJ Other Parts Discussed in Thread: LP3878 , LP3879 Hello TI Team,
is it possible to take an LP3879 LDO (for example 1.2V fix) instead of the LP3878 (Adj) and change the voltage devider to get an Output voltage of 1.5V or 2.5V?
BR …
Part Number: LP3878-ADJ Hi TI team
LP3878MRX-ADJ/NOPB will be discontinued, so I am looking for replacement parts.
Since Re-Artwork is difficult, is there an alternative part with the same Pin Configuration and Package?
The required specifications are…
Part Number: LP3878-ADJ Good morning, I am writing about a doubt that arose while reading the LP3878MR-ADJ datasheet.
In the component datasheet, on page 3, it is written
DO NOT CONNECT. Device pin 2 is reserved for post packaging test and calibration of…
Part Number: LP3878-ADJ Hi TI team,
For CLS PN 78P3215 (TI MPN: LP3878SDX-ADJ/NOPB ), we want to know the temperature range of heat dissipation when this component is under the normal operation conduction? urgent , thanks.
Part Number: LP3878-ADJ
Hi TI E2E team,
This is Ben Wang from Celestica Songshan Lake, need TI team to advise the following questions, thank you.
When we used TI part with MPN LP3878SDX-ADJ, found different impedance value between pin2 and pin3, some…
Part Number: LP3878-ADJ Hi Expert,
Looking into LP3878-ADJ Spec definition of Adjust pin voltage.
There are test conditions defined for 0.98V~1.02V.
But no test conditions defined for 0.99V~1.01V.It do confused the engineer.
Pls advice the test conditions…
Part Number: LP3878-ADJ What is the capacitance of the output capacitance? Diodes need to be added between input and output.
If it is related to the actual circuit, can you provide the calculation formula?
Part Number: LP3878-ADJ Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models Hi,
I downloaded the uncrypted model but when I want to run by Tina it notifies an error .SUBCKT D_D1 1 2
Would you please lt me know the reason?
I…
Part Number: LP3878-ADJ Other Parts Discussed in Thread: LP3878 , What does the suffix NOPB of LP3878 MRX-ADJ/NOPB generally mean? What is the difference between LP3878 MRX-ADJ and LP3878 MRX-ADJ/NOPB?
Part Number: LP3878-ADJ
Regarding the LP3878-ADJ datasheet section 7.4.1. It states:
7.4.1 Operation With VOUT(TARGET) + 2 V ≤ VIN ≤ 16 V The device operates if the input voltage is equal to, or exceeds VOUT(TARGET) + 2 V. At input voltages below…