Part Number: LP3996 Other Parts Discussed in Thread: LP5996 Dear Sir,
I am using Dual Linear Regulator LP3996. I am facing an LP3996 failure. Input is 5V and output also I am getting 5VDC in both channels. Cab you let me know the reasons for failure…
Part Number: LP3996 Other Parts Discussed in Thread: TLV751 Dear Sir,
Instead of LDO: LP3996_1, we are looking for an alternative part for a buck converter with a Power-On Reset function. (If current ratings are a little different then also please suggest…
Part Number: LP3996 Other Parts Discussed in Thread: TLV710-Q1 , , TLV751 Hi,
Could you please recommend an alternative device for LP3996 and TLV710-Q1 that has a lower Iq? I can't find any other device than those devices I have mentioned. My required…
Part Number: LP3996-Q1 I would like to confirm output voltage value of LP3996-Q1.
In the datasheet, this IC has the programable output voltage setting.
If we request 1.8V/1.8V, can you provide it?
And about the voltage setting program, how do you…
Part Number: LP3996-Q1
Hi,
Could you provide required ESR spec for LP3996-Q1?
In the datasheet, there is just min, max.
Please provide the ESR including frequency range.
Thanks.
Part Number: LP3996 A few questions regarding the LP3996 dual regulator:
1. What is the internal reference voltage? Seems like it must be < 1.0V.
2. What is the value and (probably sloppy) tolerance of the internal resistor biasing the Cbypass pin…
Other Parts Discussed in Thread: LP3996 Hi, so I am interested in using the LP3996, which is a dual output LDO regulator. I am wondering about how to do reverse battery protection though, as the datasheet doesn't say anything about that.
The device…
Hi Kelly,
We do not have an LDO that will provide all three outputs in a single device. We do have multiple dual and single output LDOs that may be able to fit your requirements depending on your Vin, Iout, and PCB space requirements. Please provide…
Hello Tsukui-san,
With FPGA's their actual power needs vary depending on the clock speed and other variables.
Therefore many times TI does not have a design for a specific FPGA.
One good way to build a design is to use Webench FPGA Architect.
…
Hi,
I've attached the 2013 User's Guide for power products. Starting on page 53 you will find a selection of PWM controllers. many of these teh frequency can be varied according to external criteria.
As an example if you use a UC3842 it is a simple…