Part Number: LP5024 We selected the LP5024(RSMR) to be the main LED driver on the main board of a small lighting device. The board includes a ATTINY3217-MNR MCU running the driver software and communicating with the LP5024 via the i2c bus.
We have verified…
Part Number: LP5813 Hi!
I was interested in new LP5813. But it is much more complicated from software side.
Do you provide some drivers?
If I buy evaluation, do you have some gui to play with leds on board?
Thanks
Part Number: LP5024 Hello,
I'm reaching out to confirm if the LP5024 is our most up-to-date cross for NXP's PCA9626B,118? If there are newer alternatives that would be better suited to replace the current devices in use please let me know! Thank…
Part Number: LP5024 Hello, My customer plans to use LP5024 at the following conditions.
Vcc=3.3V
RIREF=7.35Kohms (ISET=10mA)
In this case, which value should Max_Current_Option bit be set, 1 or 0? Or, ISET =10mA is much smaller than either IMAX 25.5mA…
Part Number: LP5024 Hello, My customer would like to drive total 24 LEDs individually.
Can they use LP5024 to do this?
With LEDx_Bank_EN=0, each LED can be controlled independently and luminance is controlled by both PWM and dc-voltage as desired? Best…
Part Number: LP5024 Other Parts Discussed in Thread: LP5861 Hi team,
Is the OUTx pins of LP5024 only supporting 5.5V abs max? Are there no OVP, right?
Regards,
Hayashi
Part Number: LP5024 Is there any rise time limitation for the input voltage to the VCC pin?
(In the case of two pattern, EN connect to VCC, and EN not connect to VCC)
Is there no problem with extremely slow rise time for input voltage?
Best regards, …
Part Number: LP5024 Dear team, Can you help us clarify questions? How to fully use 12-bits resolution of PWM in LP5024?
But, the registers are 8-bits only. From the datasheet, it says
Many Thanks,
Jimmy