Part Number: LP5569 Hi support team, I have a question about register settings.
I am gathering information from the device's D/S and EVM documents, accessing the LP5569 from the MCU via I2C, writing commands to the SRAM, and running it, but the RGB LED…
Part Number: LP5569 Other Parts Discussed in Thread: LP5813 Hi, I am searching for a way to ramp an output to a relative position. As the ramp instruction uses relative values, I don't think this is what I need. For example, I would like to change the…
Part Number: LP5569 Other Parts Discussed in Thread: LP5813 I try to LP5569's dimming
How can I run dimming??
I want the led to be dimmed by sending just one command
please check below my code.
<code>
HAL_StatusTypeDef ret; uint8_t tValue…
Part Number: LP5569 Other Parts Discussed in Thread: TEST2 Hello, I want to use LP5569 dimming control
I read all of guide but I can't.
Help me!!!
===============================================================================================
below…
Part Number: LP5569 Hi! I was considering using LP5569 to drive 3 separate segments of a 12V RGB LED strip (each segment has 3 LEDs in series for each color). Can external 12V be used to power ONLY the LEDs as long as the currents flowing into the driver…
Part Number: LP5569 Other Parts Discussed in Thread: LP5523 , Hi,
I need help regarding the control of led driver LP5569, via linux driver. We have included a kernel code for LP5569 which is similar to the kernel code of LP5523 (leds-lp5569.c), as shown…
Part Number: LP5569 Other Parts Discussed in Thread: LP5018 , LP5009 , LP5813 Hi, TI support team
Please respond to inquiries received from customers.
- Please explain the functions listed below.
- Please explain in detail about Autonomous animation control…
Part Number: LP5569 Hi TI team,
I was working on a project to blink and dim LEDs using LP5569. While doing that I was not able to put the lp5569 to charge pump 1.5x mode,
where I'm able to use the auto mode charge pump and it is working…
Part Number: LP5569 Other Parts Discussed in Thread: SEGGER , , In my project, I am interfacing lp5569 with ST MCU STM32G031K8 and using Segger Embedded studio for development. I am gettting NACK from I2C Slave LP5569. Following is startup sequence
Turn…