Part Number: LP5912-Q1 Other Parts Discussed in Thread: LP5907-Q1 , LP5907 , TPS7A21-Q1 , LP5912 Dear team,
It is similar question of e2e below, but it is for LP5912-Q1. https://e2e.ti.com/support/power-management-group/power-management/f/power-management…
Part Number: LP5912-Q1 Other Parts Discussed in Thread: LP5912 Hello E2E Experts,
Good day.
We are using the LP5912Q3.3DRVRQ1 but there are some serious issues. The IC shorts to ground during start up.
Nominal load is less than 100mA. System works fine…
Part Number: LP5912-Q1 Hi Expert,
I see in LP5912-Q1 datasheet that "This device is available with fixed output voltages from 0.8 V to 5.5 V in 25-mV steps.". Does it mean that LP5912-Q1 has 0.8V, 0.825V, 0.05V......5.45V, 5.475V and 5.5V output voltage…
Part Number: LP5912-Q1 Hi,
Good Day.
In the datasheet for this part, it states on Page 5 that the dropout voltage is not a valid condition for output voltages below 1.6V. Since this part is a fixed output LDO of 1.1V, what does this note mean?
Let me…
Part Number: LP5912-Q1 Other Parts Discussed in Thread: LP5912 Hi,
Is this part susceptible to latchup?
Do you have or aware of radiation test data (SEE, TID)
Is the part bipolar technology
Part Number: LP5912-Q1 When using this chip LP5912-Q1 to reduce voltage from 3.3V to 1.8V and 1.5V, what should be set respectively?Is there a reference circuit?
Part Number: LM1117 Other Parts Discussed in Thread: LP5912 , TPS709 , TPS7B7701-Q1 , TPS7B4256-Q1 , TL1963A , TPS7A45 , TPS706 Hi team,
Does TI have some feature like this? the integrated back-to-back diode of LDO?
Like the below block. SGM2205.
Due to customer…
Part Number: LP5912-Q1 Hi Experts,
Datasheet suggests that the pull-up resistor at PG pin should be 10-100kohm, can customer use 2.15kohm here? Because the PG pin is connected to the PORST pin of MCU, which has an internal 15kohm pull-down resistor. If…