Part Number: LP8556 Other Parts Discussed in Thread: LP8552 Hello,
I ask about LP8556TME-E05.
My customers hope to use their own settings of the product in EEPROM at the factory line and then load that setting.
Q1. In the data sheet there is…
Part Number: LP8556 Hi
My customer has question.
Can I change the content of EPROM for LP8556?
The customer saves the contents once set and wants to maintain the setting contents even when VDD = 0.
Regard
T Kishi
Part Number: LP8556 Does a calculation spreadsheet or design tool for the LP8556 exist?
I would need the LP8556 with the following configurations:
Vin = 2.9 - 4.2VDC
Vout = 10 white Leds in series per channel, 28 - 34VDC
1. 4 channels active with…
Part Number: LP8556 On a new project we have a bad feedback from the field as we have a lot of Lp8556 broken (on power on the Vldo is quiet null and becomes hot at 70°C without any regulation and no digital interface available).
As the main power supply…
Part Number: LP8556 Hi
My Customer has question.
Is there a document that explains the operation of each register of "EPROM Memory MAP" of LP8556? There are some points that are not listed in the data sheet and I can not understand what kind of action…
Other Parts Discussed in Thread: LP8556 , LP8863-Q1 We have questions about LP8556.
In datasheet p.1, Maximum LED current is 50mA.
• Up to 50 mA Per Channel
But in datasheet p.3 Device Options,
Maximum LED current is 20/23/25mA
Please…
Part Number: LP8556 Hi Team
My NB ODM customer use SLOPE function as 500mS, and when touch the power-off key, SOC will first give a BRT[7:0] value down to 0 first and then do the EN pin off or turn off BL_CTL function.
But we will see the LED turn…
Other Parts Discussed in Thread: LP8556 art Number: LP8556
Hi,
We have meet LP8556 BL flicker issue, as initial verify result, seems it caused by output current ripple not stable.
Even when Vin= 4.4V or 3.6V, current ripple ~15mA.
And when Vin…
Part Number: LP8556 Hello,
I have a few questions that I need help answering.
1. Can TI pre-program the EPROM on the LP8556 for orders >2500? If it is possible, what information would need to be provided?
2. What are some suggested inductor part…
Part Number: LP8556 Hi Team, I would like to ask about VBOOST_RANGE. Which is recommended VBOOST_RANGE=0 or VBOOST_RANGE=1 if VBOOST is 21V(TYP) in my customer's application? I would also like to know the reason. Best Regards, Yaita / Japan disty