Other Parts Discussed in Thread: LP8556 , LP8556TM-EVM Dear all:
My customer worry about the thermal issue when use LP8556 BGA package. They want to take a look at how our layout on
LP8556TM-EVM board do this. So, Can you help get the PCB layout of…
Other Parts Discussed in Thread: LP8556 Hi,
Using LP8556-E09, with IMAX set to 23mA but I need a maximum brightness of 25mA to drive my LED strings.
Is it correct to do my calculation as show below?
"1111 1111 1111" (8bit CFG0 (LSB)+ 4bit CFG1 …
Part Number: TPS61196 Other Parts Discussed in Thread: LP8556 , TPS92380 Hi team,
My customer is considering TI’s LED backlight driver products for their application, which will be used in monitor equipment. They have multiple models, and the specifications…
Part Number: LP8556TM-EVM Other Parts Discussed in Thread: LP8556 Tool/software: Hello,
I am an FAE at a distributor that handles TI products. My customer is currently evaluating the LP8556 EVM. Among these, we would like to confirm the VIN voltage…
Part Number: LP5813 Other Parts Discussed in Thread: LP8556 , LM3535 Tool/software: Hi team,
Are there any LED drivers with the following specifications?
Boost function (3.3V to 5V)
6-channel individual control
Control current: 30mA
Current…
Part Number: LM3509 Other Parts Discussed in Thread: LP8556 Tool/software: Hi Team,
I have a application to connect the 60 LED's to My system. I have input voltage of 12 V
LED Rating If= 700 mA ~ 1 A Forward Voltage = 3.2 V.
Can TI Suggest a suitable…
Part Number: LM36274 Other Parts Discussed in Thread: LP8556 , TPS65132 Hello,
We have a problem in LM36274 debugging.
The LM36274 can work well when PWM disabled.
But the LM36274 does not work when the 75HZ PWM signal is input.
So we would like…
Part Number: LM36274 Other Parts Discussed in Thread: LP8556 ,
Hi Team,
just want to check on several questions.
1. what's the meaning of LED step ration in below? and what does below picture means?
2. in below picture, why doe headroom is step…