Part Number: LP87524J-Q1 Other Parts Discussed in Thread: IWR1843AOP Hello,
I would like to use LP87524J-Q1 for IWR1843AOP, and I have the following questions about LP87524J-Q1.
1) Does "PGOOD indication signal" output after all Vout (Vout1-4) is stable…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: PEET-GUI Hello TI team,
I am trying to calculate the Power dissipation for the PMIC IC.
I can calculate conduction losses by using the Rds-ON value mentioned in the datasheet.
But when I need to…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: AWR1843AOP , , LP87745-Q1 , LP87745 Hi Team,
The customer is designing 77GHz RADAR module with AWR1843AOP and LP87524J. But they are trying to change from LP87524J to new PMIC with ISO 26262 functional…
Part Number: LP87524J-Q1 Hi,
we are working with a customer that wishes to minimize capacitance on their PCB and have determined that they do not need the B0 rail but they do want to keep using this particular PMIC. Is it possible to leave pins 8,9,10…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: IWR6843AOP , I delevop a PCB with IWR6843AOP a I want to use LP875224J-Q1 to power it without I2C communication. The schematic are the following
I have the following question about this IC:
1. The…
Part Number: LP87524J-Q1 HI
I am a Hardware Design engineer we have the below regulator schematics and have manufactured around 20 boards, but on few we are experiencing the below issue.
on PIN 10 SW_B0 output is 0V only on few boards having this issue…
Part Number: LP87524J-Q1 ●[LP87524J-Q1] PIN " CLKIN "
Described in 7.3.2 Sync Clock Functionality in DATASHEET of LP87524J -------------------------------------------------- -------------------------------------------------- --------- The nominal…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: LP87524-Q1 Hi~
I can't find LP87524J IBIS on the TI website.
Where can I get the LP87524J-Q1 IBIS model?
Part Number: LP87524J-Q1 PMIC [LP87524J-Q1] OTP configuration for Function PIN - ENx (GPIOx)
I have the following questions to ask:
1) Register "EN1_PD, EN2_PD, EN3_PD": Set the pull-down resistor to enable or disable.
[Q1] Does this setting…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: IWR6843AOPEVM , According to the datasheet the default output voltage at the SW_B3 is 2.3V? Is that correct? (Page 44 BUCK3_VOUT = (0xCA-0x9E)*0.02V + 1.42V)
Schematic of IWR6843AOPEVM Rev F uses…