Part Number: LP8764-Q1 Tool/software: Hi,
Is it possible to configure the LP8764-Q1 with a power sequencing of BUCK1+BUCK2 in multiphase with 1V output, BUCK 3 and BUCK 4 as 3.3V and 1.8V respectively. I need a sequencing as 3.3V should generate first…
Part Number: LP8764-Q1 Tool/software: Hi Team,
Please share symbol and footprint file for part number "LP876441B1RQKRQ1" in eCADSTAR format.
Thanks,
Jitendra
Part Number: LP8764-Q1 Tool/software: Hi Team,
Are these below part available. please share datasheet. if not available suggest alternate.
1. PTPS659414F4RWERQ1
2. P876441A1RQKRQ1
Regards,
Jitendra
Part Number: LP87644Q1EVM Other Parts Discussed in Thread: LP8764-Q1 , DRA821 , TPS6594-Q1 in Use's Guide: Powering DRA821 with TPS6594-Q1 and LP8764-Q1
GPIO5 of LP8764-Q1 at table 5-7, says input, but actaul EVM/reference design GPIO5 is used to…
Part Number: LP8764-Q1 Tool/software: I found two E2E threads accurately describing my issue, but neither one has a resolution.
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1334146/lp8764-q1-i2c-issues…
Hi,
NABIL KERBILA said: The device connected to the Primary PMIC is a SOC, The SOC can already deliver two different adresses , but we have to know wich adress we have to put to choose the LP8764 device , i did not find the informaiton on the datasheet…
Part Number: LP8764-Q1 Other Parts Discussed in Thread: DRA821 , Tool/software: Hello,
My customer is using LP876441B1RQKRQ1 as one of the power supplies for DRA821.
The components they use require non-China flow.
Are there any non-China flow device…
Part Number: LP8764-Q1 Tool/software: Hi Expert,
Have a nice day! I have question need BU team’s support:
For LP8764-Q1, it’s max Iout of each BUCK is 5A:
Support need:
Could BU team help to test the performance of this device on full load…
Part Number: LP8764-Q1 Tool/software: For LP8764-Q1 register set, is there a way to do an register dump and read everything together at once, and then being able to put it in a structure to be able to compare with the config file settings
Also, I…
Part Number: LP8764-Q1 Tool/software: Hi team,
Do we have the graph of switching frequency vs input voltage? I would like to confirm the variance of switching frequency when input voltage is low. I am looking for like the graph below.
Best regards…