Part Number: LSF0204 Other Parts Discussed in Thread: PCA9306 , , LSF-EVM When I use LSF0204 HSPICE Model downloaded from the webside, HSPICE shows the error massage as the attached picture. It looks like HSPICE cannot find pca9306__die.
Could you show…
Part Number: LSF0204 Other Parts Discussed in Thread: TXU0304 , TXU0104 , TXU0204 , TLV3501 Hi Team, I am using LSF0204 and circuit is . I am getting output with offset of 2.2V. May I know the reason and which pull up resistors needs to tune. Input of LSF0204…
Part Number: LSF0204 Hi Team,
I have a query in LEVEL Translator part No; LSF0204RUTR for Resistance On Measurement.
So, in the above datasheet, given the Voltage of 0V and output current of some mA, How to source load with 0V input voltage and some…
Part Number: LSF0204 Hi,
There is no description of VIH, VIL, VOH, and VOL of input/output pins other than enable in the data sheet.
The input/output pin has a FET configuration that turns the signal on and off, and the high level goes through a pull…
Part Number: LSF0204 Hi all,
I'm using LSF0204 to translate logic(PWM) from 1V8 (A side) to 5V(B side).
However, I'm measuring the B side output and it appears that the output at B side are still 1V8 (but the same logic as A side). All of 4 channels…
Part Number: LSF0204-Q1 Hi Team,
Good Day,
We are planning to use LSF0204-Q1 in Our design.
We have requirement of level shifting MDC,MDIO signals from 2.5V to 3.3V.
We want to know the propagation delay while translation.
In the datasheet we can able…
Part Number: LSF0204-Q1 Hi TI Team,
We are using LSF0204-Q in our circuit for level translating the 1.8V signal to 3.3V signal. The 1.8V supply is from a LDO and it is connected to the VREFA and 3.3V supply is connected to the VREFB. There is a pull…
Part Number: LSF0204 Hi,
I have some questions about LSF0204 level shifter.
In datasheet, recommended pass transistor current is 64mA.
And, pull-up resistor should limit the current through the pass transistor when it is in the ON state to about 15mA…
Part Number: LSF0204-Q1 Other Parts Discussed in Thread: SN74LVC2G66-Q1 , TCA9517-Q1 , SN74LVC2G17-Q1 Can we use this part as buffer, by connecting Vref_A and Vref_B at the same voltage level?