Part Number: SK-AM62A-LP Hello There,
Visteon BSP team has both AM62A EVM and AM62x EVM (SKEVM PROC114E1) from TI.
AM62A supports one LVDS channel. Is that possible to connect a Display to the AM62A EVM through DSI connector by connecting any hardware…
Part Number: LVDS-18B-EVK Dear sirs,
I have to complain because I bought an lvds-18b-evk and I found on it two very large errors.
Fortunately I was able to solve by myself but I think it is not serious to sell boards with this kind of quality.
The board…
Part Number: SN65DSI83 Other Parts Discussed in Thread: SN65DSI84 Hi Sir/Madam,
I'm working on NXP IMX8M MINI EVK board on LINUX environment. We are working on the PANASYS LVDS display which is an custom display, for converting the MIPI-DSI…
Part Number: LMX2594 I'm using the #1Nos LMK04828B and #2Nos LMX2594RHAR in my design to provide #4Nos phase aligned sampling clocks from LMX to my device.
I referred some EVK and mapped the LMK to LMX as shown in the attachment. And i have some…
Part Number: CDCE6214-Q1 Other Parts Discussed in Thread: CDCI6214 , CDCE6214 Hi TI team,
CDCE6214TWRGETQ1 is used for one of our design. We have observed some difference between datasheet and EVK user guide.
LVDS AC coupled termination as per datasheet…
Part Number: DS90UB949-Q1EVM Other Parts Discussed in Thread: DS90UH949-Q1EVM
Hello members, I am using a 1024x8 bits EEPROM (AT24C08A) with the DS90UB949-Q1EVM kit. The external EEPROM is placed on the position of "U3" in the evaluation kit. I have DELL…
Hi Krunal:
I change sdk version to 08.06.00.42
And tried following steps:
(1) add "name_overlays=k3-am625-sk-oldi-panel.dtbo" to uEnv.txt
(2) run these 2 cmds:
root@am62xx-evm:~#/etc/init.d/weston stop
root@am62xx-evm:~#kmstest
I get following…
Part Number: PROCESSOR-SDK-AM62X Hi,
How do i change the pixel clock for LVDS and RGB on am62x EVK?
I would like to change the RGB888 to RGB565, do i need to do any kernel changes?
I would like to change LVDS 8-lane to 4-lane, do i need to do any kernel…
Hi Krunal,
> I am curious why you are running 20+ instances of memtester
We are running 20+ instances of memtester to verify our DDR configuration.
> and attaching a HDMI monitor.
On our custom hardware, an LVDS display is always enabled. We discovered…
Hello Pierre
Thank you for the query.
Pierre Buffo said: I should also mention that I am working with the AM6548 EVK (IDK version) with the TI display kit.
Could you share the board version details.
Have you had a chance to revie the EVM user guide?
Is…