Part Number: MAX232E Hi
I am using an MAX232E in a motor control application. between controller and motor.
The block diagram of the product is shown below.
Some users are having trouble with MAX232E failure.
Both the motor side and the controller…
Part Number: MAX232 Hi there evrybody, I have recently ordered few MAX232N for a custom board whose function is to converter from RS232 to RS485 communication standard. While testing the behavior of the board, we encountered some complications. In order…
Part Number: MAX232 Hi
How about all the 1uF capacitors in this reference circuit
1. Can electrolytic capacitors be used?
2. Can MLCC capacitors be used?
3. The capacitance must be 1uF?
Part Number: MAX232 Can I use 1 uF/25V ceramic capacitor of size 0201 with this IC ( doc here ). Will this RS232 transceiver works OR I have to use the same value 1 uF /25V capacitors BUT bigger in size (example 0805)?
Q.2 - Does pin 16 VCC pin requires…
Part Number: MAX232E I would like to use the MAX232E to interface to the PC serial port. I used 10uF ceramic cap for C1-C4. The waveform for C1+ was from 5V to 10V, C1- was 0V to 5V, C2+ was 0V to 10V and C2- was 0V to -10V. VS+ was 8V while VS- was …
Part Number: MAX232 Hi, What will be the maximum baud rate that can be operated using the MAX232IDR ??. In the datasheet, it is given that the max. speed is 120kbps. In terms of the baud rate, what will be the max. baud rate, which can be used for this…
Part Number: MAX232 Hi team,
In customer's sysytem, SN75188NSRG4 has been used, but c ustomer is considering to repalce SN75188NSRG4 with MAX232NS in next project. Are there any concerns they need to take care about?
+/-12V is applied to SN75188NSRG4…
Part Number: MAX232E Other Parts Discussed in Thread: TRS208 , MAX208 Hi.
Please see the attached file.
I want to connect PCB1 DOUT1 and PCB2 DOUT1.
Is it possible?
If it isn't possible, do you have any ideas?
Besr regards.
MAX232E_question.xlsx
Part Number: MAX232 Dear specialists,
My customer is considering MAX232IDR and has a question.
I would be grateful if you could advise.
---
What is the maximum rating of the sink current of the driver / receiver OUT terminal?
I looked at the data sheet…