Hi Navis,
Yes, we can say that the DC jack is faulty. It is possible to replace the DC jack on the board. But. kindly ensure that this replacement should be done cautiously without peeling off the traces.
Thanks.
Part Number: MMWAVEICBOOST Other Parts Discussed in Thread: IWR6843ISK Hi,
I would like to supply the MMWAVEICBOOST/IWR6843ISK with 8V power supply instead 5V via jack connector.
So from the schematic, I deduce this way to do it
I moved the jumper from…
Part Number: IWR6843AOPEVM Other Parts Discussed in Thread: MMWAVEICBOOST , DCA1000EVM I am trying to run this demo: https://www.ti.com/video/5827389052001#transcript-tab When clicking on SPI connect I keep getting this error: [11:28:29] Status: Failed, Error…
Hi Mickael,
Could you try the below workarounds to see if the issue is with the adapter.
1. Kindly try replacing the power supply adapter with a new one and check if D11 is still glowing.
2. Make the below assembly modifications and check if D11 is still…
Hello Zuha,
Just to make sure you are aware, there is vitals signs source code available for the IWRL6432 device at the below link. The implementation is a little different but the algorithm is mostly the same as what is running on the IWR6843. Can you…
Part Number: MMWAVEICBOOST Dear,
I will supply the AWR6843AOP via the J4 connector of the MMWAVEICBOOST. The MMWAVEICBOOST supply is supplied by a 5V 3A jack charger. I need to know the maximum power that can give the MMWAVEICBOOST card on the J4 connector…
Part Number: MMWAVEICBOOST Dear,
I will supply the AWR6843AOP via the J4 connector of the MMWAVEICBOOST. The MMWAVEICBOOST supply is supplied by a 5V 3A jack charger. I need to know the maximum power that can give the MMWAVEICBOOST card on the J4 connector…
Part Number: MMWAVEICBOOST Dear,
I will supply the AWR6843AOP via the J4 connector of the MMWAVEICBOOST. The MMWAVEICBOOST supply is supplied by a 5V 3A jack charger. I need to know the maximum power that can give the MMWAVEICBOOST card on the J4 connector…
Part Number: MMWAVEICBOOST Dear, I will supply the AWR6843AOP via the J4 connector of the MMWAVEICBOOST. The MMWAVEICBOOST supply is supplied by a 5V 3A jack charger. I need to know the maximum power that can give the MMWAVEICBOOST card on the J4 connector…
Part Number: MMWAVEICBOOST Dear, I will supply the AWR6843AOP via the J4 connector of the MMWAVEICBOOST. The MMWAVEICBOOST supply is supplied by a 5V 3A jack charger. I need to know the maximum power that can give the MMWAVEICBOOST card on the J4 connector…