Part Number: MSP430FR2633 Other Parts Discussed in Thread: MSP-FET , Hi,
I designed my own board with MSP430FR2633. I use MSP-FET Flash Emulation Tool. This tool has programming pins and uart interface to communicate with uC. Is it possible to use the…
Part Number: MSP-ULTRASONIC-DESIGN-CENTER Other Parts Discussed in Thread: MSP430FR6043 Good day!
I'm using the "Ultrasonic Sensing Design Center" software. The lowest resonance frequency that can be entered on the user interface is 780 kHz.…
Part Number: MSP430FR5043 We have driven the 200Khz utlrasonic truanducor by MSP430FR5043 and made the product for sales. 200Khz utlrasonic truanducor is OK now.
But the 200Khz utlrasonic truanducor size is too big. So we want to change to a smaller size…
Part Number: MSP-ULTRASONIC-DESIGN-CENTER Hello Team,
My customer is currently developing a ultrasonic flow sensor and therefore they would like to have the source code of the "Ultrasonic Sensing Design Center". Is it possible to receive the source code…
Part Number: EVM430-FR6043 Other Parts Discussed in Thread: MSP430F5528 , UNIFLASH Hello,
I'm working on the " Optimized Ultrasonic Sensing Metrology Water Flow Measurement Reference Design" project on EVM430-FR6043. I built and ran the code…
Part Number: MSP430FR2633 Setup: Communication with the design center via IC bulk transfer via Captivate ISO adapter to Captivate PGMR.
The channel bar of the electrode is displayed, so the deflection that there is a touch. However, the interface always…
Hi zrno soli ,
In my case when starting the supply voltage was in the range > 2.4 V Vcore and MCLK could work normally.
Then the voltage drops to 2.16 V (what will happen in this case)?
Example code we use
PMM_setVCore(PMM_CORE_LEVEL_3);
…
Part Number: MSP-EM-DESIGN-CENTER Other Parts Discussed in Thread: EVM430-I2040S
Hello everyone,
This question came up recently, so I wanted to provide some guidance in case others had the same question. Currently, EMDC supports AC RMS and peak measurements…
Part Number: CAPTIVATE-ISO Hello all, I use the Captivate Development Kit with the MSP430FR2633. Since I want to run the board on battery in the future and still read out the values from the Design Center, I wanted to use the Captivate-Iso board. Unfortunately…