Part Number: MSP430F5438A-EP Other Parts Discussed in Thread: MSP-FET , TUSB3410 , MSP430F5438A Hi,
I'm trying to get the MSP-EXP430F5438 (Rev 03) board working as described in the documentation (slau263i). Hardware/connections are:
IC = MSP430F5438A…
Part Number: MSP-EXP430F5438 Tool/software: Code Composer Studio Dear team
I am using MSP-EXP430F5438 & MSP430F5438A and i want to do FFT Calculation.
I use Sine signal (frequency: 1545HZ; phase: 0; amplitude: 100mv),
1). Which port of the MSP-EXP4…
Hi Together,
I m the developer and i m having the board MSPM0G3507 and CC2564MODNEM. To connect these two, BOOST CCEMADAPTER is used. From TI side, they have developed sdk kit for CC2564 is with MSP-EXP430F5529 , MSP-EXP430F5438 , DK-TM4C129X . Unfortunately…
Part Number: MSP-EXP430F5438 I have recently purchased an MSP-EXP430F5438 Experimenter's Board, and am trying to set up my environment before the board arrives. Getting into the user manual mentioned the MSP-FET for programming. Code composer has an option…
Part Number: MSP-EXP430F5438 Hi,
Im currently working on a project were I have to read ECG values using a MSP-EXP430F5438. I have been provided with ECG electrodes which provides voltages through a 3.5 mm pin and now I am wondering how to read those voltages…
Part Number: MSP-EXP430F5438 Hello,
I have an MXP-EXP430F5438 board and an MSP-FET/MSP430 Flash Emulation Tool which I have been using in a old-ish computer with 64-bit Windows 7, building the MSPEXP430F5438(A) Example Software ( SLAC227 )... no problems…
Part Number: MSP-EXP430F5438 Hi All,
For USB driver installation , it says it is compatible for both 32 bit or 64 bit Windows PC. I tried installing in Windows 10 64 bit , but it failed . Can someone help to resolve this issue as early as possible.
My…
Part Number: MSP-EXP430F5438 Tool/software: Code Composer Studio Hi All,
I have been using RealwavfileXCPU.xls file to convert .wav Audio files to MSP430 compatibale hex files to Play Audio with MSP430F4358A.
However, I see some additional buzz noise…
Part Number: MSP-EXP430F5438 Tool/software: Code Composer Studio I am new going to start working with MSP-EXP430F5438 board, please suggest whether to work on windows or ubuntu.
Thanks for your reply Britta,
Just FYI - I had originally downloaded the example code from the link provided in the MSP-EXP430F5438 User Guide ( www.ti.com/.../slac227 ).
So after reading your comment I downloaded the MSPWare and imported the CSS project…