Part Number: MSP-EXP432P401R I am running into some errors while trying to compile code on CCS, I would very much appreciate it if i could get in touch with an engineer. The code and projects run perfectly fine when I save it as a .c file but when I change…
Part Number: MSP-EXP432P401R Hello,
I would like to test battery operation with LaunchPad. So, I disconnect 3V and 5V from the power rail, but how to interface SWD and USART if the battery voltage is varying from 3.7V to 3.0V.
Regards,
Laszlo
Part Number: MSP-EXP432P401R Upon arrival, I opened up the box containing the TI-RSLK-EVM and MSP-EXP432P401R and plugged it into my computer in my engineering class. I noticed that the board was not lighting up the green LED at the top but my classmates…
Part Number: MSP-EXP432P401R Tool/software: Code Composer Studio My project use MSP430 test fixture + CC256xCQFN-EM boards to tune RF parameters serval years before.
it used HCItester tool to run .bts script files for checking RF performance.
Now we need…
Part Number: MSP-EXP432P401R I have developed firmware for battery charging on the BQ25713 which works perfectly fine when I run it on the eval board MSP432 but I constantly face issues when trying to run it on my individually designed board. I constantly…
Part Number: MSP-EXP432P401R Hello everybody, this might be a stupid question, but how do I change the display I acctually want to access? I have two UART Displays and due to the standard defintion
Display_Handle hSerial = Display_open(Display_Type_UART…
Part Number: MSP-EXP432P401R I installed a copy of Code Composer Studio 10.3 on a Linux host. Then, I connected my board MSP-EXP432P401R to its through USB cable. When I tried to test the connection to my board, it failed.
How do I correct it?
[Start…
Part Number: BOOST-LP5569EVM Other Parts Discussed in Thread: MSP-EXP432E401Y , LP5813 , LP5569 Hi support team, According to the original question, MSP-EXP432P401R is currently unavailable and MSP-EXP432E401Y is not applicable to BOOST-LP5569EVM. Is there…
Part Number: MSP-EXP432P401R Hi, Good day. Our customer would like to use the MSP-EXP432P401R and they have several inquiries about the ADV of this device. Kindly refer to their questions below. 1. What is the sampling rate of the inbuilt ADC? 2. How may…
Part Number: MSP-EXP432P401R Dear all TI Engineers and Experts,
I am trying the Launchpad MSP432P401R TI Driver factory code Deep Sleep Power Mode but the result was many orders of magnitude larger than the result shown in TI's manual.
Are there something…