Other Parts Discussed in Thread: ENERGIA CCS V10 won't show imported projects in the project explorer. I'm trying to use the MSP EXP432P4111. Can anybody help?
Part Number: MSP-EXP432P4111 HI team
I am looking for the reference manual of MSP432P4111 but seems like everything related to that device have broken links. I meant the descriptions of functions and registers for each peripheral and core.
I got that link…
Part Number: MSP-EXP432P4111 I am just looking for the demo source code for the msp432p4111.
It is very close for what I have to do, and cannot find the C files in the Resource manager, or on the website
Part Number: MSP-EXP432P4111 Hi,
We have a weird intermittent BSL boot load problem where the BSL seemed to sync but always responded with 0x0, success, which should not occur when sending a bad password to erase and unlock memory.
I built the BSL in "debug…
Part Number: MSP-EXP432P4111 Hi,
there are 2 .cmd files for the source for MSP432BSL_1_01_00_00 for the launchpad, 401r
one is msp432p401r_debug_flash, which loads the BSL at address 0, for debugging
the other is msp432p401r.cmd, which loads the BSL where…
Part Number: MSP-EXP432P4111 Hi,
I needed to creat a bespoke version of the ubuntu scripter that talked to the BSL on a bespoke board because of error messages that had no detail.
I am working with a launchpad first because the lab setup makes it difficult…
Part Number: MSP-EXP432P4111 Hi,
I started with flash loading a .txt loadable file from the Arm Hex Utility, size about 20K bytes. no problems using the documents and bsl-scripter-linux-64.
At some point in development, the .txt file became over 40K…
Part Number: MSP-EXP432P4111 Hi team,
The problems start in the installation of MSP432P4 SimpleLink SDK ... it doesn't show up in the software folder.
p/n MSP-EXP432P4111 with BOOSTXL-EDUMKII ... and I get errors following the pre-work instructions…
Part Number: MSP-EXP432P4111
Hi,
I am having some issues with the basic stuff of I2C communication protocol on the MSP432. I am running a code in CCS for a basic master mode write function. This is my code at the moment:
MAIN.C
#include <I2CComm.h>
…
Part Number: MSP-EXP432P4111 Hi, I build the "oad_firmware_update" example combined with the cc2640r2 as SNP. Works ok but I'm confused when reading the manual:
In the "OAD_firmware_update" project the MRDY is an output from theCC2640R2…