Part Number: MSP-EXPCC430RFX I am using msp-expcc430. Through the
MspExp430F5137RxUserExperience.c
/*******************************************************************************
*
* MspExp430F5137RxUserExperience.c - Main User Experience…
Part Number: MSP-EXPCC430RFX Dear TI engineer
I am using msp-expcc430RF development kit. However, it suddenly broke. When connecting to the power source 2V, the current is higher than 1 A. When using the meter to measure the Vin and GND pin, it shows…
Part Number: MSP-EXPCC430RFX
Tool/software: Code Composer Studio
I found an example of the msp-expcc430rfx user experience. But I couldn't find any project file in ccs!!!!!
So I had to create a new project and import the experience.c. After adding…
Hello Li,
How did you download the code to the board successfully? Was it working before you programmed it?
It looks like there are switches on the board that control which MCU you are programming, either the base board or the satellite board. Have…
Part Number: MSP-EXPCC430RFX
The CAL_ADC_20T30=1029 ,CAL_ADC_20T85=1896. The temperature is calculated by the formula provided in datasheet IntDegC =(SavedADC12MEM0-CAL_ADC_20T30)*((85-30)/(float)(CAL_ADC_20T85-CAL_ADC_20T30))+30; The IntDegC=64 when…
Part Number: MSP-EXPCC430RFX The problem I have is that I have a peak in the measurement (voltage in a temperature probe (NTC)) equivalent to the ambient light sensor.
I have verified that voltage peaks are generated in Vref, which distorts the measurement…
Dear All,
I am working on a project using MSP-EXPCC430RF4 EVM ,i had downloaded the MSP-EXPCC430RFx user experience setup & when ever i tried to run the .exe file ,i am experiencing application error.
"Error : Error in Action execute Action
…