Calum,
The only eval board for the MSP430F2274 is the 38-pin target board which comes with free code size limited tools not free tools.
MSP430 38-Pin Target Board: http://www.ti.com/tool/msp-fet430u38
My suggestion would be to have the customer use…
Hi,
Thanks for the reply. I was downlaoded this IAR Embedded Workbench Kickstart software from the website which prompted from installed CD. The software descrption as stated below where the GUI without MSP430F4152 device. Any idea for me to download the…
Steve,
You could use the USCI SPI port of MSP430 to communicate with the AIC3254.
The output from PurePath (a .h header file) can be compiled in the MSP430 code. You would need to parse the data structures and translate them into SPI commands. More…
Other Parts Discussed in Thread: MSP430G2955 , MSP-TS430DA38 Hi community member,
Please provide your advice in order to resolve the following phenomenon.
[Phenomenon]
When added one line as below in the interrupt routine of Time A, not outputted the expected…
Hi Gaston,
which MSP430 device do you like to connect to (bacause I do not know what slauc138l.pdf is for)?
Pls note that the values of R1 (Pull-Up for RST line) and C1 are device-dependant; detailed information on the recommended values can be found…
I have not heard of any such issues with the MSP430F2274. You might want to do the following: 1. Remove everything that the MSP430 is connected to and just have the board that the MSP430 is on.
2. Tie P3.x to Ground on your board and see what happens to…
Other Parts Discussed in Thread: MSP430F2252 To make a long story short, I have a subroutine that provides the timing to drive a stepping motor which outputs square waves on P4.4 - P4.7.
Essentially when I run the code posted below with the dev board…