I un-installed CCS (well, as far as it got before the program printed "Critical Error" and aborted).
remove all files in the ti directory, then installed the latest version of CCS
I still get the:
MSP430: Error initializing emulator: MSP-FET430UIF…
Part Number: MSP430FR6989 Hello, I have been attempting to use my MSP430 however whenever I try to debug or flash the program onto the board I consistetly get an error : Error initializing emulator: MSP-FET430UIF is already in use and I'm unable to change…
Part Number: MSP430F6726 Hello,
Our board manufacturer is using Elprotronic FET-Pro430 and MSP-FET430UIF to program a MSP430F6726 via Spy-Bi-Wire. He is asking why it takes almost two minutes to erase and reprogram the flash memory. He updated the memory…
Part Number: MSP430F5519 MSP430F5519 code composer studio “Version 12.0.0” shows the error “The debug interface to the target is secure” when debugging with JTAG “MSP-FET430UIF”.
While debugging using code composer…
Part Number: MSP-FET Other Parts Discussed in Thread: UNIFLASH
Hi,
Writing is done using the following debugger. When I use ① MSP-FET430UIF, I can't write software, but ② MSP-FET can write normally.
I'm using Uniflash to write, but I can't write…
Part Number: MSP-FET430UIF I get the following error when I download the application using MSP-FET430UIF.
MSP430: Error connecting to the target: Unknown device.
The second and fourth pins of the JTAG both supply the same error.
What are the reasons for…
Part Number: MSP430FR2355 Is it possible to connect the MSP-FET430UIF via virtual com port with CCS? In CCS there is an option "UARTConnection". But no UART can be selected. regards Hardy