Part Number: MSP430FR2433
Hi,
Which library file and header do I use for the MSP430FR24433 with CCS 12.5.0? I installed it but it's not an option in CCS products.
Regards,
-Mike
Part Number: MSP-IQMATHLIB Hello,
I am working in AD measurement which prints real value in Voltage. The basic theory is to calculate an LSB in IQ20 and in the measurement cycle only multiply with (integer subtracted with zero point integer). My problem…
Part Number: MSP-IQMATHLIB Hi
I'm currently using IQMathLib in my project. And I encountered a problem with _IQ29div.
The dividend was 0.0027313 and the divisor was 0.0101318, but the output was 0.1347891.
And I tested another set of number, 0.0148468…
Hi,
We usually use IQ format data to represent decimal data in MSP430. You can refer to this link for a better understanding of IQ format data.
https://www.ti.com/tool/MSP-IQMATHLIB
Best regards,
Cash Hao
Hi,
Here is one solution, you can convert the float data into a fixed point data and then send out the fixed point data. The receiver will convert the fixed point data back to float data.
The _IQ fixed point format data can be used here. You can refer…
Part Number: MSP-IQMATHLIB Tool/software: Code Composer Studio How can I use CCS V9 and IAR V7+ to create a library similar to IQmathLib that MSP430 can use. I found some resources, but they are out of date. I can't see them.
www.iar.com/.../
processors…
I see. Thanks for confirming and explaining the use case here.
I think there are two options here. I do not know what devices are used in your overall system, but the immediate option that you should explore is to install the MSP-IQMATHLIB , which has functions…
Part Number: MSP-IQMATHLIB Similar to the issues here: http://e2e.ti.com/support/microcontrollers/msp430/f/166/p/348830/1830267#1830267
If I pass a negative string to _atoQ() the polarity of the result depends on if there is a decimal point included.
…
Hi, David
Sorry, I didn't have enough information.
Supplement.
toshiharu.yoshie said: In this case, will it be an IQN (IQ5 or less) that will not reach 16777216 even if it is doubled?
Regarding this, when I looked at the user guide (page 10, Table…