Part Number: MSP-EXP432E401Y Hi, I am facing a weird issue, I am using Launch develop kit2 and the Scalable-PMICs-GUI. when i connect the developing kit to a windows platform with the GUI, the hardware is being recognized by the app, but on a linux system…
Part Number: MSP430FR50431 Other Parts Discussed in Thread: MSP-FET Hi,
I have a custom board that contain the msp50431, and i use the MSP-FET to burn into it a new code.
I connect the pins according to your recommendation:
https://e2e.ti.com/support/microcontrollers…
1) So if I have something like a JTAG connector, like on the EVM, in my design When I connect my board with the MSP-FET to the computer Will the USS recognize? And can I use this software?
2) i mean to the USS, yes
but dont forget that i have the msp-fet…
Part Number: MSP-EXP430G2ET Other Parts Discussed in Thread: MSP430G2553 I worked on the MSP-EXP430G2 and it was fine. Recently I bought MSP-EXP430G2ET boards.
So, while I can perfectly program my MSP430G2553 mcu with the MSP-EXP430G2 on both MAC and Linux…
Part Number: MSP-FET Good morning,
I looked in the forum but could get an answer.
I ordered 3 new MSP FET (the black ones) and connected them. They are recognize as a com port, everything is fine.
I tried to use them thru MSP430 flasher; They rebooted…
Part Number: MSP-FET430UIF Tool/software: Code Composer Studio I bought MSP-FET430UIF, Rev.2.0.6.
When I connect the emulator with my computer, multiple errors occur.
First, it says "Error Initializing Emulator" and asks me to update the emulator.…
Hello Bryce,
You can try to check your device and IDE according to the following suggestions,
1). Check the device manager of your computer whether the MSP-FET is recognized and connected;
2). Check if multiple MSP-FET are connected to the computer;
…
Part Number: MSP-EXP430FR5969 Other Parts Discussed in Thread: MSP-FET Hi,
When I first started using the MSP-EXP430FR5969 eval kit, I used the USB interface and everything worked fine.
I then started using the JTAG interface and that worked as well…
Hello,
The USB interface of MSP-FET connects it to the computer, and the 14-pin connector of MSP-FET provides access to the MSP debugging simulation port.
Perhaps you can first try to check if the computer correctly recognizes the UBS interface of the…
Part Number: MSP-EXP430FR5994 I am trying to use MSP_EXP430FR5994 Launchpad kit for SD read/write operation. Now the kit is not detected by the PC, no communication ports are available(it is showing that the USB device not recognized). The red led(LED101…