"After moving the "Result" assignment into the interrupt I am still having trouble reading in an analog voltage. The analog voltage is a DC voltage that I can vary between 0-250 mV "
You can change analog input voltage range by…
Part Number: RF430FRL152H Other Parts Discussed in Thread: MSP-FET Hello,
In my previous question I explained that I had fabricated a custom tag using the RF430FR152H chip, and I was able to program it over the air using the TRF7970A reader. However, in…
Part Number: MSP430L092 Other Parts Discussed in Thread: MSP-FET , CCSTUDIO Tool/software: Code Composer Studio Was using CCS 9.3.0 under Windows 10 Pro to program a MSP430L092, with the target device in a MSP-TS430L092. This was done as part of seeing…
Part Number: TIDM-RF430-TEMPSENSE Other Parts Discussed in Thread: MSP-FET , RF430FRL152H Hello,
I would like to program the TIDM-RF430-TEMPSENSE with a JTAG programmer, as my program cannot be uploaded over the air, because of a failure causing bricking…
Part Number: MSP430L092 Other Parts Discussed in Thread: MSP-FET , CCSTUDIO , MSP430WARE , MSP430F5528 , MSP430F2274 Tool/software: Code Composer Studio Using CCS 9.3 under Ubuntu 18.04.3 LTS created a project for a MSP430L092, with the target device in a …
Ki said: I am trying to reproduce this locally, and currently looking for the EVM to try out. I don't have a RF430FRL152, but have repeated the same error with a MSP430L092, in a MSP-TS430L092 Target Board connected to a MSP-FET.
Where RF430FRL152 an…
Hello Ruan,
Yes, the MSP-TS430L092 target board and the MSP-FET are supported by CCS. The legacy MSP-FET430UIF is not recommended for new designs (NRND). The 14-pin connector of the MSP-FET plugs into the L092 Active Cable board that's connected to the…
Hello Alex,
Thank you very much for your help, we really appreciate !
With regards to the JTAG, I’m not sure if the TEST connection is needed, since I think that it is needed when JTAG pins are shared I/O pins, which is the case here, but at the…
Hello Judes,
Did you base your schematic design off of the MSP-TS430L092 Target Socket Board? Since the MSP-FET operates from 1.8 to 3.6 V and the MSP430L092 from 0.9 to 1.65 V you need to incorporate hardware similar to that of the MSP-TS430L092 Active…
Hi Robert,
I wanted to give you a quick update on this. The engineer who wrote the APIs and the loader.h file is back from his leave and I had a chance to sync up with him on the issues you're experiencing.
It looks like there is some initialization…