You could purchase either the MSP-TS430PZ100B or MSP-TS430PEU128 target boards to begin evaluating these devices, or if you are interested in e-metering applications then there are several more EVMs to consider (EVM430-F6779, EVM430-F6736, or EVM430-F67641…
Hi Jace,
Thank you for pointing out! I understood that there is no problem with the setting of the user's guide.
I tried also the sample code of LPM 3 and the result was as follows.
MSP-TS430PZ100B
Customer's Board
LPM3 example
No phenom…
Hello Janani,
All this should be possible, but it will take some time and work to implement.
On the software side, the F5xx and F6xx are similar devices, and the MSPMATHLIB library that's used in the TIDM-3DGRAPHICS-QVGA design is supported on both…
Part Number: MSP430F6736A Other Parts Discussed in Thread: MSP430F6779 , MSP-TS430PZ100B , , MSP-FET , MSP430F6736
Hi anyone
I have a coin battery back up to the MCU via AUXCC3. (The intention behind the battery backup is purely to keep the RTC & Backup RAM…
Other Parts Discussed in Thread: MSP-TS430PZ100B , ENERGYTRACE , MSP-FET , EVM430-F6736 Hello,
Could you please advice how to demonstrate ILPM4=1.6uA ?
Let me explain my status:
- I built a board as the attached schem
- The sample code "MSP430F673X_LPM4…
Other Parts Discussed in Thread: MSP-FET , MSP430F6733 , MSP-TS430PZ100B [ MSP430F6733IPN ] MSP-FET Unable to connect to target
We are facing communication problem between MSP-FET and target (MSP430F6733).
We have two boards, one is customer board, and…
Other Parts Discussed in Thread: MSP-TS430PZ100B
Hi,
I will use MSP430F677x 100pin device.
In D/S it is recomned to use MSP-TS430PZ100B.
So,I have some quetions of AUXVCC and GPIO connections.
So,Let me know Jumper settings and other pins.
I checked AUXVCC…
Other Parts Discussed in Thread: MSP-TS430PZ100 , MSP430FR5969 , MSP430F5659 , MSP-TS430PZ100A , MSP-TS430PZ100D , MSP-TS430PZ100B , MSP-FET There appears to be an external oscillator on the board, but it says "not assembled". Also, when setting up…
Other Parts Discussed in Thread: MSP430F6747 , MSP-TS430PZ100B , MSP-TS430PEU128 , MSP430F6736
Hi all,
Now I would use 100pin-MSP430F674x.
In product folder, It it recommend to use 128pin socke, not 100pin.
http://www.ti.com/product/MSP430F6747/toolsso…
Part Number: MSP430F6733 Other Parts Discussed in Thread: MSP-GANG , MSP430G2452 ,
Team,
I tried to use BSL-SCRIPTER to open the locked JTAG of MSP430F6733,[I can use MSP-GANG to do the erase with the BSL function]. I used a msp430G2 LP[msp430G2452] and…