Part Number: MSP430F5335 Hellow,
I have some questions about RTC.
*DVCC=3.3V, Reset Pin(96pin) is pulled up 47k, and conected to GND through capacitor.
(MSP430™ Hardware Tools.pdf Figure B-68. MSP-TS430PZ100C Target Socket Module, Schematic)
VBAT…
Hi Kary,
In the code you shared, if there's an oscillator fault flag, it won't continue to the part of code that toggles the LED. Looking at the picture you shared, how you've soldered the crystal to the target board isn't how we recommend doing it. Since…
Jace,
Thank you for your reply!
We are connected over USB to the MSP-FET Flash Emulation Tool. We are using the full JTAG connection. The board is powered externally, not thru the MSP-FET. Power was on and stable well before starting MSP430Flasher…
Hi!
Unfortunately there is no LaunchPad with the MSP430F5359 assembled - there is one that has the MSP430F5529 on it: MSP-EXP430F5529LP. Maybe this is suitable for evaluating, too. There is also the generic MSP-TS430PZ100C that can be used with MSP430F5x…
Hi Pratheep,
For the correct development tools please refer to the MSP-TS430PZ100C EVM and MSP-FET.
All previous versions of CCS below v7 are free of charge, and CCS v6.1.3 is the first release to offer support for Windows 10: processors.wiki.ti.com…
Part Number: MSP430F5359 Tool/software: Code Composer Studio I am using MSP430F5359 with the MSP-TS430PZ100C development tool within CCS and am using the ADC12 module with MSP driver library.
I would like to trigger the ADC12 sampling every 4ms using TimerA…
Part Number: MSP430F6438 Tool/software: Code Composer Studio Hi There,
I use the MSP-TS430PZ100C (REV1.1) with MSP430F6438 MCU.
I have 2 questions here.
Q1. I want use XT1 with a 32.768KHZ crystal. The resistor R6 and R8 are 0. The crystal come with the…
Hi Aaron,
According to Table 1-1 in the MSP430 Hardware Tools user's guide , the MSP430F535x devices are supported by the MSP-TS430PZ100C target board. The MSP430F543x devices are supported by the MSP-TS430PZ5x100 target board (and the MSP-EXP430F5438…
Other Parts Discussed in Thread: MSP430F6438 Hi Dear,
I have USB programmer and MSP-TS430PZ100C demo board, and they works very well with CCS6.1. I can download and debug code on MSP430F6438.
When I connect to my PCB, The ccs6.1 can not connect to it…
Part Number: MSP430F5338 Other Parts Discussed in Thread: MSP430F6438 , MSP-FET Tool/software: Code Composer Studio A microprocessor that I am using appears to be causing Code Composer Studio to crash when attempting to debug it.
I am working with two…