Hi Pravin,
As you can see in the Hardware Tools User's Guide www.ti.com/lit/pdf/slau278 on p. 84 in the BOM for the MSP-TS430RGC64B, the QFN11T064-006 socket is manufactured by Yamaichi (not TI). You will have to find a local distributor or online…
Hi Kummi,
I tested on the MSP-TS430RGC64B target board and an MSP430F5310 device, and I was successfully able to use BSL with MSP-FET.
Your connections look correct, and I'm really sorry this issue is stretching so long. As a note, if you use the TI target…
We have some more data about this issue. The conclusion is MSP430F5341/2's behaviour is different from other F5xx devices like MSP430F5310.
In order to cross-check we tried to test the same on TI's target boards with other F5xx devices and the MSP430F5341…
Other Parts Discussed in Thread: MSP430F5328 Hello,
I am working with an MSP430F5328 and I would like to know the power consumption while reset is active. I am using the MSP-TS430RGC64B target board. On the target board I have only a 20MHz crystal, all…
Jeffrey Westgeest said:
I have tried the blinking led program, but every time I try to start the debugger I get the message:
Error connecting to the target: Unknown device.
You are using the MSP-TS430RGC64B with MSP430F5328. Here are a few things you…
Hello Todd,
The 53xx devices will be supported by the 64-pin QFN target board. MSP-TS430RGC64B
There are currently plans for a 48-pin board, however it will not support the 53xx devices.
MSP430 Starter Kits: Programmers, Target Boards
Regards,
…
Other Parts Discussed in Thread: MSP430F5308 Hi all,
I try to modify the BSL from application note 450 to work with the I2C peripheral. I can download a small test program using IAR compiler. However, when i try to use BSL sequence (reset and test pins…
Other Parts Discussed in Thread: MSP430F5328 I use the MSP-TS430RGC64B EVM board. I want to estimate the max SPI speed of MSP430F5328.I choose the USCI_A0 as SPI Master,and USCI_A1 as SPI slave.and i use Dupont line to connect the used pins.I configure…
Sorry I was not generous with details.
I could reproduce the situation on a msp430f5308, in the development module MSP-TS430RGC64B ( http://www.ti.com/tool/msp-ts430rgc64b ). See code below.
Is the hardware version binary coded decimal? Does 0x12…