Other Parts Discussed in Thread: MSP430G2553 , MSP430F5528 , MAX3232 Hi,
I'm using the MSP-TS430RGC64USB target board to implement the MSP430F5528. I've used the Launchpad previously to implement UART on a MSP430G2553 that would spit out the data on a COM…
Hi Nicole,
The image you attached did not come through.
I think you need to set P5SEL.2 to 0 to configure P5.2 & P5.3 as outputs.
You will need P5SEL &= ~BIT2; //SEL set GPIO P5.2 & P5.3 sets as input/output
Also, looking at the schematics…
To eliminate our hardware I have set up the same test using TI MSP-TS430RGC64USB dev kit and the results were the same. I did have to correct the port pins to 0 and 1 as per my previous post which proved the examples provided are incorrect.
…
Part Number: MSP430F5510 Other Parts Discussed in Thread: MSP430F5529 , MSP-FET , MSP430FR5739 Hello
I am having difficulty in getting the UART BSL loader to work on the MSP430F5510. This is what I have tried:
1. Using the TI dev board: MSP-TS430RGC64USB…
Part Number: MSP430F5528 Other Parts Discussed in Thread: MSP-FET , MSP-FLASHER Tool/software: Code Composer Studio Hi,
I'm using the MSP-TS430RGC64USB with MSP-FET.
When I connect my MSP-FET to CCS 10.0, it starts configuring Debugger, it says (Error…
Hi Susan,
I would suggest the section 28.2.3 Voltage Reference Generator of the device User's Guide for how to configure the ADC reference.
The MSP-EXP430F5529LP LaunchPad is an inexpensive, simple microcontroller development kit for the MSP430F5529…
Hi Tao
I have try it on my side with this software and the LED blink demo with no problem.(I use the msp430f5514 with the MSP-TS430RGC64USB target board)
Here I have two suggests:
1. make sure the customer make right operation to invoke the BSL: Pull…
Part Number: MSP430F5528 Tool/software: Code Composer Studio I am new to the MSP430 software, I am using the MSP430F5528 with the MSP-TS430RGC64USB breakout board for testing.
I am trying to configure Port PU for output, to do a basic LED blink function…
Ki said: The properties for this breakpoint appears to be the cause of the crash. Can you remove all breakpoints (clear all entries in the Breakpoints view) and try to relaunch the debug session? I found that the workspace in which the crash was originally…