Part Number: MSP430-IEC60730-SW-PACKAGE Hi,
We are using MSP430 IEC60730 software package. For class B compliance, do we need to run both POST() and PST() tests or one of these is enough?
Part Number: MSP430-IEC60730-SW-PACKAGE Other Parts Discussed in Thread: MSP430FR2633 Hi,
We are using MSP430FR2633 for one of our projects and implementing IEC60730 SW Package in it
The following memory partition is used in the example provided in the…
Part Number: MSP430-IEC60730-SW-PACKAGE Hi,
For IEC60730 Class B compliance, is interface level validation required? If yes does the MSP430-IEC60730-SW-PACKAGE, have APIs to validate external UART interface.
Part Number: MSP430-IEC60730-SW-PACKAGE Other Parts Discussed in Thread: MSP430FR2433 Hi,
We are using MSP430FR2433 in our product which requires IEC60730 compliance. We are planning to use MSP430-IEC60730-SW-PACKAGE library for Class B compliance.
Wanted…
Part Number: MSP430-IEC60730-SW-PACKAGE Hi,
We are designing a system which requires IEC60730 certification.
The question is whether IEC60730 certification can be achieved by just using the IEC60730 SW packages or are there any hardware features required…
Hello,
Pascal Chambon said: I have the same message "no code associated with..." when trying to force-enable these breakpoint
There appears to be some issue with the source code correlation. Would you be able to provide the project with the issue…
I am running into the same problem encountered previously when trying to install CCS 12 including the msp430 support onto windows 11. Looks like an know issued but it has been always resolved via E2E chat.