Part Number: MSP430F167 Other Parts Discussed in Thread: TCA6424A , TIDM-THDREADING Hi,
My application is to detect the AC voltage presence using Continuous high or low signal.
(I got the same issue with MSP430F167 and TCA6424A IO extender)
I am using…
Part Number: MSP430F167 Tool/software: Code Composer Studio Hello,
I have an old program (almost dated 2004 and updated in 2014) used in one of our electronic boards having msp430f167. I want to make some changes, however I get many errors. I am missing…
Part Number: MSP430F167 Tool/software: TI C/C++ Compiler As part of a MSP430F167 code development process the .out file from CCS was disassembled by dis430.exe.
A "designed to be stand alone code section" was then inspected for any calls/jumps outside…
Part Number: MSP430F167 Other Parts Discussed in Thread: USB2ANY
Hi
I got a new MacBook Pro and put Parallels + Windows 10 on it. USB2ANY driver based GUIs work just fine. But MSP430F167 based GUI doesn't work.
I've read several threads on this topic…
Part Number: MSP430F167 Tool/software: Code Composer Studio
Hello,
I have rebuilt an old code in CCS. However when i use TI compiler i get the following error.
When i use the GNU compiler, the program compiles to give a .hex file with a warning…
Part Number: MSP430F167 Why does conformal coating peel from this part? Conformal coating is adhering to remainder of parts of this PCA but not the MSP430F167IPM .
Are molds sprayed with silicone when cover is molded?
What is the surface energy of the…
Other Parts Discussed in Thread: CC430F5137 , MSP-FET , MSP430F167 , MSP-TS430PM64 , MSP430F5510 I have built a board with the MSP430F167. I am attempting to program it with CCS 6.1.2 with windows 10 and 7 (I have two computers). At one point and time I was…
Other Parts Discussed in Thread: MSP430F167 Having trouble with MSP430F167 as slave, because it will not recognize and ACK it's own address. I do get the start interrupt if enabled. But because of the errata I2C16 in http://www.ti.com/lit/er/slaz148a…
Other Parts Discussed in Thread: MSP430F167 , MSP-TS430PM64 Our customer is using the MSP430F167. He is having problems programming it.
"Much of the time now it just says the fuse has been blown, but there's no way for my emulators to do that. The rest…
Other Parts Discussed in Thread: MSP430F167 In an earlier version of CCS (CCS2.0) for MSP430, a standard C file, containing code and tables of constants was compiled and linked into a specific flash memory region in a MSP430F167 known as section ".new_boot…