Part Number: MSP430F2013-EP Hello, can you tell me if the active mode current incorporates the SD16 current as well? As the active mode current changes with clock speed, does that also change the SD16 current consumption?
Thank you for your time!
Dav…
Hi Christopher,
We also have the catalog version of the MSP430F2619S-HT, www.ti.com/product/MSP430F2619.
At the same please take a look at the following devices :
www.ti.com/.../msp430g2332-ep or www.ti.com/.../msp430g2332
www.ti.com/.../msp430g2231…
Hi Claudio,
The MSC1201 is still active. If the product web page shows the device as 'Active' then there are no plans to obsolete the device. If the product page shows 'NRND' then that the device is not recommended for new designs. Generally…
Other Parts Discussed in Thread: LM25037 , UCC28089 , MSP430F2013-EP Hi
Can LM25037 use as controller for Modified Square Wave Inverter.
- Freq_mod=55Hz, Vin=300V, Vout=220Vac.
- App: Inverter equipment for car option.
(I know that the gate drivers is required…
Other Parts Discussed in Thread: MSP430F2013-EP Hello together,
I have a question in using the MSP430F2013-EP at the maximum temperature of 125 °C. I intend to use a 32 kHz oscillator instead of a 32 kHz crystal (crystal function only up to 105 °C, datasheet…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave