Part Number: MSP430F235 Hello,
I am designing an ultra low power Gas Meter Pulse Counter using reed switch. My system works well, counts Meter Values and save each hour in EEPROM.
Now I need some additional functionality to develop in it.
calculate Qmax…
Part Number: MSP430F247 Other Parts Discussed in Thread: MSP430F235 Hi team,
I have an existing project with the MSP430F235TPMR and intend to replace it with the MSP430F247TPMR.
However, the datasheet shows a difference in the memory map of the RAM:
…
Part Number: MSP430F235 Hi,
In our design based on the MSP430F235, we use the ADC12 (Vref = AVCC=3.3V and ADC12OSC is used as ADC source clock).
We notice that the values in ADC12 registers are higher than expected (let's say about +10).
I was wondering…
Part Number: MSP430F235 Other Parts Discussed in Thread: LDC1614 , LDC1614EVM Tool/software: Code Composer Studio Hi,
I need to use an external coil with LDC1614 boost from Ti, asking about if i have use an external coil which have a core inside it like…
Part Number: MSP430F235 Other Parts Discussed in Thread: LDC1614 Tool/software: Code Composer Studio Hi,
i need to use external coil with LDC1614 sensor and i have some questions about the specifications of the coil.
1. if the coil has a core inside it…
Part Number: MSP430F235 Hi Team,
My customer is using MSP430F235, but with some questions want to double confirm, thanks for your support.
1. if they didn't set the SVSCTL, what will be the default brownout voltage?
2. Where can customer set proper…
To access the Result registers you need at least one cycle if using indirect addressing modes as per datasheet section 11.2.4. I think I understand but I'm not certain
I am using the MACS as the last in a series of calcs. Xsquared + Y squared + Z…
Other Parts Discussed in Thread: MSP430F235 Using Usci in Uart mode, after some time of working properly, suddenly the output levels of the UTXD0 inverted (Steady state = '0' ; Start bit = '1' and so on).
Now even after power cycle and…
Other Parts Discussed in Thread: MSP430F235 Hello,
I m using msp430f235 micro controller.
It does not contain test pin in it, And I m programming it using 4 wire JTAG.
I have issue that my controller is not being programmed by JTAG using CCS6.
The error…
Configuration 1:
Change to configuration 2
This is the picture of configuration 2:
Can anyone tell me if I can change the configuration 1 to the configuration 2? Configuration 1 is a crystal with 2 terminal. Configuration 2 is a crystal oscillator…